This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 processor with 4 sample and hold circuit

Hi Team,

A customer is looking for a C2000 processor with at least 4 sample-and-hold circuits for 6 phase PMSM motor control applications. Do we have a processor with this feature?

Regards,

Danilo

  • Hi Danilo,

    No, we do not have a C2000 device with an ADC that supports 4 S+H circuits, directly.

    However, I would highly recommend looking at the F2837x series.  This device instead has 4 independent ADC modules, each configurable to enable sampling simultaneously with the other ADCs.
    (therefore, from a system-perspective this C2000 device would resemble a device that has a single ADC with 4 S+H circuits)

    With this configuration, the F2837x can also simultaneously convert the analog signals meaning that overall system latency can be reduced.


    Specifications for this ADC can be found in its device datasheet.


    Thank you,
    Brett

  • Hi Brett,

    Thank you for your suggestion.

    Regards,

    Danilo