Part Number: TMS320F28379D
Hey Team,
I have a customer that is using the TMS320F28379DPTPQ, which has 3 pins, FLT1, FLT2, and ERRORSTS, that are defined as 'no connect' in the datasheet.
For deep space application they are trying to avoid "floating metal" since it is possible that charge can build up over time. Our thinking is that if these pins are output pins, then they are fine, but if they are inputs with weak pull-up/down or other means of weak bias, then there could be a concern about the charge being able to change the state of the pin, and that could be bad.
What are these pins, and if the above risk is there, what can we do externally to pull them high or low or bias to something benign.
Best,
Dajon McGill