Part Number: TMS320F28035
Hello,
I'm currently working on a project and I'm using the SCI of the F28035 (standard) to send instructions to another microcontroller. The problem is when I use a the setChannel function (posted bellow) the SCI gets stuck after sending the first intruction "mac set ch status 8 on\r\n" (\0 is the stop character). When the function is called again to turn channel 9 on, the SCI sends '9on' characters almost non stop.
void setChannel(int channel){
char *out;
char chnn[2];
ltoa(channel, chnn, 10);
out = strcat("mac set ch status ", chnn);
out = strcat(out, " on\r\n\0");
scia_msg(out);
}
The variable chnn used to be a char* but the function didn't recognize the buffer and the variable value never changed, so I changed to a char[2] and it worked but it introduced this new problem. did I program something wrong?.
Thanks in advance,
José.