Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D
Tool/software: Code Composer Studio
Hi,
I am using Launchpad XL F28379D , By using that established RS485 communication between Motor driver and Controller board . Communication is controlled by switch , for my application want to activate driver one by one .when I am started with first driver its works fine , so then I have started second drive to be activate. Unfortunately my boards gets turned off. So I left the all connection and checked continuity between the all the pins . My SCI - RX pin gets Shorted with 3.3V in board pins.
I have checked my Switch pins delivers 3.3v and 0v during operations.
I have use level converter in between the controller board RS485 module .
Here terminal resistor also added in module itself .
Thanks & Regards,
Rani