Tool/software: TI C/C++ Compiler
Hi,
I use hex2000 to convert my .out to .b00.
hex2000.exe path is "C:\ti\ccs930\ccs\tools\compiler\ti-cgt-c2000_18.12.5.LTS\bin"
This is my command: hex2000.exe "inputFileName" -boot -sci8 -b
I set all FLASH by ALIGN(8) in 2838x_flash_lnk_cpu1.cmd.
Attach my cpu1 .cmd file
MEMORY
{
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x088000, length = 0x000002
BOOT_RSVD : origin = 0x000002, length = 0x0001AF /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x0001B1, length = 0x00024F
RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* RAMD0 : origin = 0x00C000, length = 0x000800 */
/* RAMD1 : origin = 0x00C800, length = 0x000800 */
// This section is set for Ramfunc2
RAMD0D1 : origin = 0x00C000, length = 0x001000
/* ===== Ram sectors ===== */
/* RAMLS0 : origin = 0x008000, length = 0x000800 */
/* RAMLS1 : origin = 0x008800, length = 0x000800 */
/* RAMLS2 : origin = 0x009000, length = 0x000800 */
/* RAMLS3 : origin = 0x009800, length = 0x000800 */
/* RAMLS4 : origin = 0x00A000, length = 0x000800 */
/* RAMLS5 : origin = 0x00A800, length = 0x000800 */
/* RAMLS6 : origin = 0x00B000, length = 0x000800 */
// This section is set to CLA program
RAMLS0LS6 : origin = 0x008000, length = 0x003800
// This section is set to CLA data
RAMLS7 : origin = 0x00B800, length = 0x000800
/* RAMGS0 : origin = 0x00D000, length = 0x001000 */
/* RAMGS1 : origin = 0x00E000, length = 0x001000 */
/* RAMGS2 : origin = 0x00F000, length = 0x001000 */
CPU1RAMGS0GS1A : origin = 0x00D000, length = 0x001D00
CPU1RAMGS1BGS2 : origin = 0x00ED00, length = 0x001400
/* RAMGS3 : origin = 0x010000, length = 0x001000 */
/* RAMGS4 : origin = 0x011000, length = 0x001000 */
/* RAMGS5 : origin = 0x012000, length = 0x001000 */
/* RAMGS6 : origin = 0x013000, length = 0x001000 */
CPU1RAMGS3GS7A : origin = 0x010100, length = 0x004500
/* RAMGS7 : origin = 0x014000, length = 0x001000 */
/* RAMGS8 : origin = 0x015000, length = 0x001000 */
/* RAMGS9 : origin = 0x016000, length = 0x001000 */
CPU1RAMGS7BGS9 : origin = 0x014600, length = 0x002A00
/* RAMGS10 : origin = 0x017000, length = 0x001000 */
/* RAMGS11 : origin = 0x018000, length = 0x001000 */
/* RAMGS12 : origin = 0x019000, length = 0x001000 */
CPU2RAMGS10GS13A : origin = 0x017000, length = 0x003800
/* RAMGS13 : origin = 0x01A000, length = 0x001000 */
/* RAMGS14 : origin = 0x01B000, length = 0x001000 */
/* RAMGS15 : origin = 0x01C000, length = 0x000FF8 */
CPU2RAMGS13BGS15 : origin = 0x01A800, length = 0x0027F8
// RAMGS15_RSVD : origin = 0x01CFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* Flash sectors */
/* Start : Bootloader */
/* FLASH0 : origin = 0x080002, length = 0x001FFE on-chip Flash */
/* FLASH1 : origin = 0x082000, length = 0x002000 on-chip Flash */
/* FLASH2 : origin = 0x084000, length = 0x002000 on-chip Flash */
/* FLASH3 : origin = 0x086000, length = 0x002000 on-chip Flash */
/* End : Bootloader */
/* FLASH4 : origin = 0x088000, length = 0x008000 on-chip Flash */
/* FLASH5 : origin = 0x090000, length = 0x008000 on-chip Flash */
/* FLASH6 : origin = 0x098000, length = 0x008000 on-chip Flash */
/* FLASH7 : origin = 0x0A0000, length = 0x008000 on-chip Flash */
/* FLASH8 : origin = 0x0A8000, length = 0x008000 on-chip Flash */
/* FLASH9 : origin = 0x0B0000, length = 0x008000 on-chip Flash */
/* FLASH10 : origin = 0x0B8000, length = 0x002000 on-chip Flash */
/* FLASH11 : origin = 0x0BA000, length = 0x002000 on-chip Flash */
/* FLASH12 : origin = 0x0BC000, length = 0x002000 on-chip Flash */
/* FLASH13 : origin = 0x0BE000, length = 0x002000 on-chip Flash */
FLASHEN1 : origin = 0x088008, length = 0x037FB8 /* on-chip Flash */
/* Can not change this memory setting (Bootloader) */
FLASHN_APPINFO : origin = 0x0BFFC0, length = 0x000030 /* on-chip Flash */
// FLASH13_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000800 */
CPU1TOCPU2RAM1 : origin = 0x03A000, length = 0x000300
CPU1TOCPU2RAM2 : origin = 0x03A300, length = 0x000100
CPU1TOCPU2RAM3 : origin = 0x03A400, length = 0x000400 /* Reserved */
/* CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000800 */
CPU2TOCPU1RAM1 : origin = 0x03B000, length = 0x000300
CPU2TOCPU1RAM2 : origin = 0x03B300, length = 0x000100
CPU2TOCPU1RAM3 : origin = 0x03B400, length = 0x000400
/* CMTOCPURAM : origin = 0x038000, length = 0x000800 */
CMTOCPU1RAM1 : origin = 0x038000, length = 0x000300
CMTOCPU1RAM2 : origin = 0x038300, length = 0x000500 /* Reserved */
/* CPUTOCMRAM : origin = 0x039000, length = 0x000800 */
CPU1TOCMRAM1 : origin = 0x039000, length = 0x000300
CPU1TOCMRAM2 : origin = 0x039300, length = 0x000500 /* Reserved */
CANA_MSG_RAM : origin = 0x049000, length = 0x000800
CANB_MSG_RAM : origin = 0x04B000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
}
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : > FLASHEN1, ALIGN(8)
.cinit : > FLASHEN1, ALIGN(8)
.switch : > FLASHEN1, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
.stack : > RAMM0 /* There is stack size set in Properties->C2000 Linker->Basic Options-> -Stack */
#if defined(__TI_EABI__)
.init_array : > FLASHEN1, ALIGN(8)
.bss : > CPU1RAMGS3GS7A
.data : > CPU1RAMGS3GS7A
.sysmem : > RAMM0
/* Initalized sections go in Flash */
.const : > FLASHEN1, ALIGN(8)
#else
.pinit : > FLASHEN1, ALIGN(8)
.ebss : > CPU1RAMGS3GS7A
.esysmem : > RAMM0
/* Initalized sections go in Flash */
.econst : > FLASHEN1, ALIGN(8)
#endif
// EABI Format with no head "_"
ramfuncs : LOAD = FLASHEN1,
RUN = CPU1RAMGS7BGS9,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
ramfuncs2 : LOAD = FLASHEN1,
RUN = RAMD0D1,
LOAD_START(Ramfuncs2LoadStart),
LOAD_SIZE(Ramfuncs2LoadSize),
LOAD_END(Ramfuncs2LoadEnd),
RUN_START(Ramfuncs2RunStart),
RUN_SIZE(Ramfuncs2RunSize),
RUN_END(Ramfuncs2RunEnd),
ALIGN(8)
/* CLA specific sections */
Cla1Prog : LOAD = FLASHEN1,
RUN = RAMLS0LS6,
RUN_START(Cla1funcsRunStart),
LOAD_START(Cla1funcsLoadStart),
LOAD_SIZE(Cla1funcsLoadSize),
ALIGN(8)
CLADataLS0 : > RAMLS7
CLADataLS1 : > RAMLS7
#ifdef CLA_C
/* CLA C compiler sections */
//
// Must be allocated to memory the CLA has write access to
//
.scratchpad : > RAMLS7
.bss_cla : > RAMLS7
.const_cla : LOAD = FLASHEN1
RUN = RAMLS7,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize),
ALIGN(8)
#endif //CLA_C
/* AppInfo */
AppInfoFiles : > FLASHN_APPINFO, ALIGN(8)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
However, in hex2000 output file, my 1st block start at address 0x88008 and size 0xFFFE.
The 2nd block start at address 0x98006(0x88008 + 0xFFFE) and is not fit 128-bits alignment.
This cause my bootloader cannot write data at 0x98006 with the FLASHAPI.
How can I figure it out?