I recently migrated from the F2808 DSP to the Piccolo series, and started development on the Piccolo ControlStick. I am currently using CCS 3.3, and can successfully get a CPU Timer ISR running using the PIE vector block in RAM. I have tried several times to compile the same program from Flash, but no luck blinking the LED on the ControlStick. I have attached the project file with all necessary includes, can anyone help me or have noticed a similar issue?
-Bryan