Other Parts Discussed in Thread: TUSB3410
I am attempting to interface with the Blinking LEDs program using the General Purpose GUI with the following configuration:
- Docking-Stn USB-EMU [R3]
- F28335 controlCard R1.0
- Docking-Stn SW1 in USB position
- Using on board XDS100 JTAG emulator
- No jumpers added, switches changed etc. hardware is out of the box
The PC is connected to the Docking-Stn J3 via TUSB3410UART EVM and DB-9 to 4 pin header (SIL). The Blinking LED program successfully builds and runs with the debugger. I can control the blink rate of LD1 on the controlCard by modifying Gui_LEDPrd. The GUI is configured with the TUSB3410 COM port and the baud rate is set to 57600. When I attempt to connect to the program from the GUI LD1 stops blinking. When I then halt the debugger program execution is stuck at:
0x3FF9FA: 6F00 SB 0,UNC
Any ideas what's happening here?