Part Number: BOOSTXL-POSMGR
Other Parts Discussed in Thread: TIDM-1010
Hello there
I am thinking of using an encoder that communicates with BISS-C. However, as far as I have researched, there is no direct support for the BISS-C interface in C2000 MCUs. It is necessary to design a converter together. I have read that your BOOSTXL-POSMGR product is used as a BISS_C converter. There are some features on it that will also perform different functions. I want to make a BISS_C converter according to the "www.rls.si/.../aksim-2-off-axis-rotary-absolute-encoder" encoder that I shared this link. In my design, I will design a card with a minimum size with reference to the BISS-C converter part of your BOOSTXL-POSMGR product, of course, if the interfaces that will run this encoder are available in this converter.
1- Can I communicate with the encoder whose link I shared using your BOOSTXL-POSMGR product?
2- How can I do it for only one BISS-C converter C2000 family with reference to your BOOSTXL-POSMGR product? (You can mark and show the structures I need to put from the BOOSTXL-POSMGR schematic)
Best Regards