Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE
Hi,
I am trying to update epwm duty cycle inside CLA task on LAUNCHXL-F28379D . I have taken example cla_ex4_pwm_control for my reference, my epwm1 is running at 12.5khz and epwm2 at 8.3khz. While debugging, I am able to trigger breakpoint in CLA task but it doesn't update compareA reg value when this EPWM_setCounterCompareValue(EPWM1_BASE, EPWM_COUNTER_COMPARE_A,1000) is called.
This is my CLA task
__interrupt void Cla1Task1 ( void )
{
__mdebugstop();
EPWM_setCounterCompareValue(EPWM1_BASE, EPWM_COUNTER_COMPARE_A,
1000);
//
// Clear EPWM2 interrupt flag so that next interrupt can come in
//
EPWM_clearEventTriggerInterruptFlag(EPWM2_BASE);
}
Below code is for my CLA and EPWM init functions
//
// CLA_configClaMemory - Configure CLA memory sections
//
void CLA_configClaMemory(void)
{
extern uint32_t Cla1funcsRunStart, Cla1funcsLoadStart, Cla1funcsLoadSize;
EALLOW;
#ifdef _FLASH
//
// Copy over code from FLASH to RAM
//
memcpy((uint32_t *)&Cla1funcsRunStart, (uint32_t *)&Cla1funcsLoadStart,
(uint32_t)&Cla1funcsLoadSize);
#endif //_FLASH
//
// Initialize and wait for CLA1ToCPUMsgRAM
//
MemCfg_initSections(MEMCFG_SECT_MSGCLA1TOCPU);
while (!MemCfg_getInitStatus(MEMCFG_SECT_MSGCLA1TOCPU)){};
//
// Initialize and wait for CPUToCLA1MsgRAM
//
MemCfg_initSections(MEMCFG_SECT_MSGCPUTOCLA1);
while (!MemCfg_getInitStatus(MEMCFG_SECT_MSGCPUTOCLA1)){};
//
// Select LS4RAM and LS5RAM to be the programming space for the CLA
// First configure the CLA to be the master for LS4 and LS5 and then
// set the space to be a program block
//
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS4,MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS4,MEMCFG_CLA_MEM_PROGRAM);
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS5,MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS5,MEMCFG_CLA_MEM_PROGRAM);
//
// Next configure LS0RAM and LS1RAM as data spaces for the CLA
// First configure the CLA to be the master for LS0(1) and then
// set the spaces to be code blocks
//
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS0,MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS0, MEMCFG_CLA_MEM_DATA);
MemCfg_setLSRAMMasterSel(MEMCFG_SECT_LS1,MEMCFG_LSRAMMASTER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS1, MEMCFG_CLA_MEM_DATA);
EDIS;
}
//
// CLA_initCpu1Cla1 - Initialize CLA1 task vectors and end of task interrupts
//
void CLA_initCpu1Cla1(void)
{
//
// Compute all CLA task vectors
// On Type-1 CLAs the MVECT registers accept full 16-bit task addresses as
// opposed to offsets used on older Type-0 CLAs
//
EALLOW;
// Suppressing #770-D conversion from pointer to smaller integer
// The CLA address range is 16 bits so the addresses passed to the MVECT
// registers will be in the lower 64KW address space. Turn the warning
// back on after the MVECTs are assigned addresses
#pragma diag_suppress=770
CLA_mapTaskVector(CLA1_BASE,CLA_MVECT_1,(uint16_t)&Cla1Task1);
CLA_setTriggerSource(CLA_TASK_1, CLA_TRIGGER_EPWM2INT);
#pragma diag_warning=770
//
// Enable the IACK instruction to start a task on CLA in software
// for all 8 CLA tasks. Also, globally enable all 8 tasks (or a
// subset of tasks) by writing to their respective bits in the
// MIER register
//
CLA_enableIACK(CLA1_BASE);
CLA_enableTasks(CLA1_BASE,CLA_TASKFLAG_1);
}
void initEPWM1()
{
//
// Set-up TBCLK
//
EPWM_setTimeBasePeriod(EPWM1_BASE, EPWM1_TIMER_TBPRD);
EPWM_setPhaseShift(EPWM1_BASE, 0U);
EPWM_setTimeBaseCounter(EPWM1_BASE, 0U);
//
// Set Compare values
//
EPWM_setCounterCompareValue(EPWM1_BASE,
EPWM_COUNTER_COMPARE_A,
EPWM1_MIN_CMPA);
EPWM_setCounterCompareValue(EPWM1_BASE,
EPWM_COUNTER_COMPARE_B,
EPWM1_MAX_CMPB);
//
// Set up counter mode
//
EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_UP_DOWN);
EPWM_disablePhaseShiftLoad(EPWM1_BASE);
EPWM_setClockPrescaler(EPWM1_BASE,
EPWM_CLOCK_DIVIDER_1,
EPWM_HSCLOCK_DIVIDER_1);
//
// Set up shadowing
//
EPWM_setCounterCompareShadowLoadMode(EPWM1_BASE,
EPWM_COUNTER_COMPARE_A,
EPWM_COMP_LOAD_ON_SYNC_CNTR_ZERO);//EPWM_COMP_LOAD_ON_CNTR_ZERO);
EPWM_setCounterCompareShadowLoadMode(EPWM1_BASE,
EPWM_COUNTER_COMPARE_B,
EPWM_COMP_LOAD_ON_SYNC_CNTR_ZERO);//EPWM_COMP_LOAD_ON_CNTR_ZERO);
//
// Set actions
//
EPWM_setActionQualifierAction(EPWM1_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(EPWM1_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_LOW, //LOW
EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA);
EPWM_setActionQualifierAction(EPWM1_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
EPWM_setActionQualifierAction(EPWM1_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPB);
//
// Set up EPWM2 to
// - run on a base clock of SYSCLK
// - have a period of EPWM2_PERIOD
// - run in count up mode
EPWM_setClockPrescaler(EPWM2_BASE, EPWM_CLOCK_DIVIDER_1,
EPWM_HSCLOCK_DIVIDER_1);
EPWM_setTimeBasePeriod(EPWM2_BASE, EPWM2_TIMER_TBPRD);
EPWM_setTimeBaseCounterMode(EPWM2_BASE, EPWM_COUNTER_MODE_UP_DOWN);
EPWM_setTimeBaseCounter(EPWM2_BASE, 0U);
//
// Enabling EPWM2 interrupt at TBCTR = 0 to trigger
// CLA task
//
EPWM_setInterruptSource(EPWM2_BASE, EPWM_INT_TBCTR_ZERO);
EPWM_enableInterrupt(EPWM2_BASE);
EPWM_setInterruptEventCount(EPWM2_BASE, 1U);
//
// EPWM 1 and 2 should run freely in emulation mode
//
EPWM_setEmulationMode(EPWM1_BASE, EPWM_EMULATION_FREE_RUN);
EPWM_setEmulationMode(EPWM2_BASE, EPWM_EMULATION_FREE_RUN);
}