Part Number: TMS320F280049
Tool/software: TI C/C++ Compiler
C2000 Software/Compiler Team,
Let me preface this by saying I've read through and tried implementing the examples at:
https://processors.wiki.ti.com/index.php/Combining_executable_files
I'm trying to combine a bootloader and application out file for production programming purposes and I'm having trouble.
First I tried example 1 from the above link where you just pass all the out files to hex2000. I've tried adding and removing options like memwidth, romwidth, various load_image options and I always seem to get an error about memory ranges being out of order:
memory ranges "image_11" and "image_12" out of order
This is just one of the errors I get, but interesting to note is that the number of out of order errors I get changes based on whether I pass the bootloader or application out file to the tool first. Here is an example of how I'm calling hex2000 in the post build steps:
${CG_TOOL_ROOT}/bin/hex2000 bootloader.out application.out --memwidth=16 --romwidth=16 --load_image --load_image:file_type=executable --load_image:output_symbols=true -o ${PROJECT_LOC}/ROM/combined.out
Not being one to give up easy, I've also tried example method 3 where the application is actually linked in the bootloader using an application object file and the bootloader linker command file. This completes without errors but the application when loaded is not correct. Here is what memory should look like:
Here's what it looks like when loaded with the outfile generated using the application object file and bootloader linker file:
I'm generating the application obj file as follows:
${CG_TOOL_ROOT}/bin/hex2000 application.out --memwidth=16 --romwidth=16 --load_image --load_image:file_type=executable --load_image:section_prefix="app_image" -o app_image.obj
I originally didn't have the mem/rom width arguments but thought that might be the culprit due to how the memory looked, but there appears to be something else going on.
Can someone point me in the right direction? Thanks in advance,
Trey