This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F280049C: connect to custom Motor drive board

Part Number: LAUNCHXL-F280049C

Tool/software: Code Composer Studio

Dear team,

Please check the following issue:

Does F280049C launchpad  have to be connected to an optocoupler drive module to drive the motor drive board?

Customers need to connect non-TI motor drive boards. Do the PWM interfaces of J4 and J8 of F280049C need to be connected to the optocoupler drive module to connect to the PWM signal end of the motor drive board?