This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28232: F28232 Execution Time

Part Number: TMS320F28232
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

I am working in TMS320F28232 for Three Phase AC to DC PWM rectifier.

I have configured the PLL to operate in 150MHz. I have checked 37.5MHz frequency am getting in XCLKOUT pin.

It was configured as SYSCLKOUT / 4. so the operating frequency is 150MHz. Am i right??

My doubt is what is the cycle time??

i am doing toggle a IO pin like below.

GpioDataRegs.GPCDAT.bit.GPIO79 = 1;

VD  = 3720;

GpioDataRegs.GPCDAT.bit.GPIO79 = 0;

I am getting 840ns between ON and OFF in the IO pin. Is that right???

Should cycle time be 6.67ns for 150MHz operating frequency???

In project properties -> optimization tab -> optimization level was set at 2 and speed was set at 5.

Please clarify my doubt and give some suggestion about this...

Thanks and Regards

Vasu