Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
After succecefully building the code there are total 5 warnings which are poping up,which are as following:-
#10247-D creating output section "AdcaResultFile" without a SECTIONS specification
#10247-D creating output section "AdcbResultFile" without a SECTIONS specification
#10247-D creating output section "AdccResultFile" without a SECTIONS specification
#10247-D creating output section "AdcdResultFile" without a SECTIONS specification
#10247-D creating output section "Cla1SoftIntRegsFile" without a SECTIONS specification
I have checked couple of other threads as well like thread 1 and thread 2. I have added nonBIOS_cpu1.cmd file as well as RAM/FLASH linker cmd file. Still these warnings are coming up and ADCResultRegs are not getting updated despite of proper channel selection.
Regards,
Shamik