Part Number: TMS320F28377S
Tool/software: Code Composer Studio
Hello,
We are working on a power converter and we are using TMS320F28377S microcontroller in it. For updating firmware we use USB flash programmer given in C2000. It work fine, until we not use high voltage supply (550V DC, we are using SMPS and linear voltage regulator to convert high voltage input supply to 3.3V for microcontroller). We are getting this error (attachment ) while firmware update using USB and some times microcontroller was not detected on PC USB. We also not connect the +5V supply of PC with our PCB, only D+,D- and GND are connected . All other function's are working normally, including firmware update using SCI. So anyone face similar problem then please share possible cause and solution.