Part Number: F28M36H33B2
Hello Team,
Currently, my customer is planning to use F28M36H33B2 which has on its input an optocoupler. The Forward current of the optocoupler is like 25mA to 50mA and is written in the datasheets that the controller that the maximum buffer strength is 4 to 8mA, and in electrical specs written maximum sink current is 8mA. How they can enable this Optocoupler from the controller?
Regards,
Renan