This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335 McBSP SPI problem...

Hi all,

I configured McBSP in SPI clock mode with 8 bit data transfer.

1. When I place a data in DXR1 register, which bit is shifted out first, Bit15(MSB) or Bit0(LSB) of DXR1 register?

2. Since the SPI data transfer is set at 8-bits, is it required to shift the 8-bit data before placing in DXR1 register?