Part Number: TMS320F280049
Hi experts:
We have a new application requirement for TMS320F280049. We want to monitor the frequency drift of OSCCLK(external oscillator is selected). Furtherly, if the frequency drift is out of acceptable range, software protection should be done. I have learned that DCC can be used to detect clock frequency bust in most cases, OSCCLK is selected as Clock0. Is it possible to set OSCCLK as Clock1(which is under test)? And which clock can be selected as Clock0 in that case?
Thanks!
Best Regards
Meng