Hi Team,
As per the TRM for F2838x, the length of CLA_REGS is 48h and for F2807x it is 40h. However, in the cmd files for these processors the length is mentioned as 80h. Which of these should be followed?
Also is it ok if the lengths are mentioned as per the TRM.