Part Number: TMS320F2808
Hi,
my customer have been using TMS320F2808 for long.
Recently they've got a batch of board whose ADCRESULT will change for a fixed sampled voltage when temperature changes.
And we have found out that it's caused by the change of VADCREFM when temperature changes.
VADCREFM is 0.56V at 10C, and 0.57V at 50C.
VADCREFP is 1.31V at 10C, and 1.31V at 50C.
They want to do failure analysis since only this recently batch has such problem, but I'm not sure if the voltage we measured is out of spec since we only have typical value for internal voltage reference temperature coefficient in the datasheet.