Part Number: TMS320F28388D
Other Parts Discussed in Thread: TMDSCNCD28388D, C2000WARE, TPS62420
Team,
Can you please help with the below question?
1) According to the data sheet, each voltage supply pin (VDD, VDDIO) should be decoupled with 100nF each.
Is this a MUST or can nearby supply pins also be combined together? Any concrete advised for this?
2) Is there a breakdown of the VSS connections available, to understand which power supply or function groups they belong to?
3) Is it really necessary to connect a 22µF capacitor between VREFHIx and VREFLOx at the ADC connections for 16-bit conversion (see page 17 of SPRSP14C)?
4)I have seen from different other E2E forum post that the best document for Hardware design duidelines is the datasheet/data manual.
Is it correct?
Also can the TMDSCNCD28388D card (schematics/PCB in C:\TI\c2000\C2000Ware_3_01_00_00\boards\controlCARDs\TMDSCNCD28388D) be considered as good reference for the HW design?
For example is the TPS62420 PMIC handling the appropriate power up/down sequencing for 3V3 and 1V2?
Thanks in advance!
A.