This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: TMS320F280049 interrupt at CTR=ZERO with HRPE = 1

Part Number: TMS320F280049


I'm programming a dc/dc converter controller which have two full-bridge LLC interleaving with TMS320F280049M and I'm tring to use HRPWM.

With two LLC interleaving, ePWM1 and ePWM2 are used to generate two PWM signals with 90degree phase shift to drive the LLC separately. LLC is a resonant converter, so both period and phase need modify it's vaule every a few PWM cycles.

Because of Up-Down Count Duty Cycle Range Limitation Example (HRPCTL[HRPE]=1) TRM Figure 18-89, CTR=ZRO & CTR=PRD can't be used for AQ to generate PWM action. Since that, Why it still possible to use CTR=ZRO/CTR=PRD rigger a interrupt ? what is the exact time when the interrupted issued as there is two parts (PRD:PRDHR or TBPHS: BPHSHR)for the period and zero? 

Will the Interrupt trigger time also varies like the pwm will jitter when AQ generate action on CTR=ZRO?

  • Yes you can generate an interrupt in your setting with CTR=ZERO.

    That is the coarse step = ZERO event of the TBCTR. It has nothing to do with the high resolution part of the EPWM.

    The interrupt is triggered exactly at TBCTR=ZERO and ofcourse a couple of cycles before the ISR handler starts executing.

    Again, the jitter, if it is part of the HR and is not present on the EPWM withouth HR, no it wont be there on when the ISR is generated. 

    In general if you are using HRPWM, with period and phase control, maybe you want to add deadband later, etc... Make sure to not use AQ at ZRO/PRD. Use AQ to generate actions at CMPAU/CMPAD.

    Nima

  • Hi Nima,

    Thank you for your reply. 

    Yes, I'm trying to to use HRPWM, with period and phase control by modifying TRREM to realize phase shift in the interrupt routine triggered by ePWM1 CTR=ZRO. The Master(ePWM1) seems good, but I found some jitter on the slave(ePWM2) at some specific micro-step, say, PRD:PRDHR = 20.2 seems good, but PRD:PRDHR = 20.6 will show some jitter on the slave pwm signal (with CMPA = PRD/2, AQ using CAU set and CAD clear the pwm).

    As you mentioned above. 

    "The interrupt is triggered exactly at TBCTR=ZERO and ofcourse a couple of cycles before the ISR handler starts executing."

    In the ISR handlerthe TRREM value of both the ePWM1 and ePWM2 will be modifed as showed bellow. I want to know how this is possible to modify the TRREM value just in time for a cpu runing at 100MHz with a couples of cycles before the ISR handler and a couples of instructions to run before modify TRREM register? Or does the TRREM have a shadow register?

        EALLOW;
        if (LoadAction == 1)
        {
            //
            // This should also write to GLDCTL2 of PWM2
            //
            (*ePWM[1]).GLDCTL2.bit.OSHTLD = 1;
    
            //
            // TBCTR phase load on SYNC (required for updown count HR control)
            //
            (*ePWM[2]).TBCTL.bit.PHSEN = TB_ENABLE; 
    
            //
            // TBCTR phase load on SYNC (required for updown count HR control)
            //
            (*ePWM[2]).TBPHS.bit.TBPHS = temp_PHS;
            (*ePWM[2]).TRREM.bit.TRREM = 0x100 + temp_REM; 
            (*ePWM[1]).TRREM.bit.TRREM = 0x100; 
    
            LoadAction = 0;
        }
        else
        {
            (*ePWM[2]).TBCTL.bit.PHSEN = TB_DISABLE;
        }
    
        EDIS;
    

    Regards,

    Ruj

  • TRREM does not have a shadow register.

      

    Can you comment on the TRREM value update? I do not have the technical information on the TRREM workaround.

  • Hi Nima, 

    I still have some question about the interrupt trigger time and I think there is something different beacuse of the fraction part of the period.

    As you mentioned here :

    "So HRPWM works using "delay" elements. Meaning the HRPWM delay is not connected to a clock. There are actual delay elements which will delay the signal and you can enable a different number of elements to delay the edges of the PWM signals."

    and above:

    "That is the coarse step = ZERO event of the TBCTR. It has nothing to do with the high resolution part of the EPWM.

    Again, the jitter, if it is part of the HR and is not present on the EPWM withouth HR, no it wont be there on when the ISR is generated. "

    It seems the MEP works independently with normal resolution PWM module. The Integer part of period is determined by Timer-Counter & TBPRD register with a clock and the fraction part of period is determined by the MEP delay(with numbers shown in REM).

    Consider a situation like this: PRD:PRDHR = 10.1, the integer part is 10, so the PWM without HR works like period with 10. However, the real full period is 10.1, with time goes, the fraction part will accumulate every cycle and eventually bigger than 1, like below.

    Does the coarse part will handle the integer produced by the accumulate part of fraction ?  Will this affect the interrupt trigger period?

    Regards,

    Ruj

  • Ruj,

    For that level of detail, let me take this to design to get an accurate answer for your specific question.

    Nima

  • Hi,

    Yes, fraction accumulates over multiple cycles. Coarse step changes, intermittently, when that fraction accumulation crosses over the coarse step boundary.
    Interrupt is always generated over the coarse values (fractional part has no significance in the interrupt generation. 

  • Nina and Subrahmanya, Thank you very much for your explain.

  • Hi,

    Thank you. please close the thread.