Part Number: TMS320F280049C
Hi
I have configured a comparator to detect a fault and output is passed to DCBH of epwm1 through epwmXBAR. If a trip occurs I want EPWM1A to go low and EPW1B to go high with some dead time, to implement this DCBEVT1 (enabled one-shot trigger) is set to trigger T1 in the action qualifier. Everything looks working, but PWM outputs are not getting latched after the occurrence of an event.
In the normal condition, EPWM1A is high and EPWM1B is low, when a fault occurs EPWM1A is low and EPWM1B is high for sometime later it comes back to its original state, I have attached an image of the PWM waveform for reference (EPWM1A - Yellow, EPWM1B - Blue). After the occurrence of an event TZFLG.DCBEVT1, TZFLG.OST and TZOSTFLG.DCBEVT1 is set to 1 but I don't understand why PWMs are not getting latched after an event.
I have also attached the code for reference, please let me know if I missed any settings.
//############################################################################# // // FILE: cmpss_ex2_digital_filter.c // // TITLE: CMPSS Digital Filter Configuration // //! \addtogroup driver_example_list //! <h1> CMPSS Digital Filter Configuration </h1> //! //! This example enables the CMPSS1 COMPH comparator and feeds the output //! through the digital filter to the GPIO14/OUTPUTXBAR3 pin. //! //! \b External \b Connections \n //! - Output can be observed on GPIO14 //! //! \b Watch \b Variables \n //! - None //! // //############################################################################# // $TI Release: F28004x Support Library v1.06.00.00 $ // $Release Date: Fri May 24 03:33:32 CDT 2019 $ // $Copyright: // Copyright (C) 2019 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // Included Files // #include "driverlib.h" #include "device.h" // // Function Prototypes // void initCMPSS(void); void initEPWM(void); // // Main // uint16_t status = 0; void main(void) { // // Initialize device clock and peripherals // Device_init(); // // Disable pin locks and enable internal pullups. // Device_initGPIO(); // // Initialize PIE and clear PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_7, 2); // // Set up COMP7H // initCMPSS(); // // Set up ePWM1 to take CTRIPH as TRIP4 for its DC trip input // initEPWM(); // // Configure GPIO11 to output CTRIPOUT1H (routed through XBAROUTPUT7) // GPIO_setPinConfig(GPIO_11_OUTPUTXBAR7); GPIO_setPinConfig(GPIO_0_EPWM1A); GPIO_setPinConfig(GPIO_1_EPWM1B); // // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) // EINT; ERTM; // // Loop indefinitely // while (1) { status = CMPSS_getStatus(CMPSS7_BASE); } } // // initCMPSS - Function to configure the high comparator of CMPSS1 // void initCMPSS(void) { // // Enable CMPSS and configure the negative input signal to come from // the DAC // //UV CMPSS_enableModule(CMPSS7_BASE); CMPSS_configHighComparator(CMPSS7_BASE, CMPSS_INSRC_DAC); // // // Use VDDA as the reference for the DAC and set DAC value to midpoint for // arbitrary reference // UV CMPSS_configDAC(CMPSS7_BASE, CMPSS_DACREF_VDDA | CMPSS_DACVAL_SYSCLK | CMPSS_DACSRC_SHDW); CMPSS_setDACValueHigh(CMPSS7_BASE, 1092); // // Configure digital filter. For this example, the maxiumum values will be // used for the clock prescale, sample window size, and threshold. // CMPSS_configFilterHigh(CMPSS7_BASE, 0, 16, 15); // // Initialize the filter logic and start filtering // CMPSS_initFilterHigh(CMPSS7_BASE); CMPSS_clearFilterLatchHigh(CMPSS7_BASE); // // Configure the output signals. Both CTRIPH and CTRIPOUTH will be fed by // the filter output. CMPSS_configOutputsHigh(CMPSS7_BASE, CMPSS_TRIP_FILTER | CMPSS_TRIPOUT_FILTER); XBAR_setOutputMuxConfig(XBAR_OUTPUT7, XBAR_OUT_MUX12_CMPSS7_CTRIPOUTH); XBAR_enableOutputMux(XBAR_OUTPUT7, XBAR_MUX12); } // // initEPWM - Function to configure ePWM8 and the ePWM X-BAR to take CTRIPH as // the DC trip input // void initEPWM(void) { // // Disable the ePWM time base clock before configuring the module // SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC); //EPWM // setup the Time-Base Control Register (TBCTL) EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_UP_DOWN); EPWM_disablePhaseShiftLoad(EPWM1_BASE); EPWM_setPeriodLoadMode(EPWM1_BASE, EPWM_PERIOD_DIRECT_LOAD); EPWM_setSyncOutPulseMode(EPWM1_BASE, EPWM_SYNC_OUT_PULSE_ON_SOFTWARE); EPWM_setClockPrescaler(EPWM1_BASE, EPWM_CLOCK_DIVIDER_1, EPWM_HSCLOCK_DIVIDER_1); EPWM_setCountModeAfterSync(EPWM1_BASE, EPWM_COUNT_MODE_UP_AFTER_SYNC); EPWM_setEmulationMode(EPWM1_BASE, EPWM_EMULATION_FREE_RUN); // setup the Timer-Based Phase Register (TBPHS) EPWM_setPhaseShift(EPWM1_BASE, 0); // setup the Time-Base Counter Register (TBCTR) EPWM_setTimeBaseCounter(EPWM1_BASE, 0); // setup the Time-Base Period Register (TBPRD) // set to zero initially EPWM_setTimeBasePeriod(EPWM1_BASE, 0); // setup the Counter-Compare Control Register (CMPCTL) EPWM_setCounterCompareShadowLoadMode(EPWM1_BASE, EPWM_COUNTER_COMPARE_A, EPWM_COMP_LOAD_ON_CNTR_ZERO); EPWM_disableCounterCompareShadowLoadMode(EPWM1_BASE, EPWM_COUNTER_COMPARE_B); // EPWM_disableCounterCompareShadowLoadMode(EPWM1_BASE, EPWM_COUNTER_COMPARE_C); // EPWM_disableCounterCompareShadowLoadMode(EPWM1_BASE, EPWM_COUNTER_COMPARE_D); // setup the Action-Qualifier Output A Register (AQCTLA) EPWM_setActionQualifierAction(EPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_HIGH, EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA); // changed from High to low EPWM_setActionQualifierAction(EPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW, EPWM_AQ_OUTPUT_ON_TIMEBASE_DOWN_CMPA); // changed from low to high // setup the Action-qualifier Continuous Software Force Register // (AQCSFRC) EPWM_setActionQualifierContSWForceAction(EPWM1_BASE, EPWM_AQ_OUTPUT_B, EPWM_AQ_SW_OUTPUT_HIGH); // setup the Dead-Band Generator Control Register (DBCTL) EPWM_setDeadBandDelayMode(EPWM1_BASE, EPWM_DB_RED, true); EPWM_setDeadBandDelayMode(EPWM1_BASE, EPWM_DB_FED, true); // select EPWMA as the input to the dead band generator EPWM_setRisingEdgeDeadBandDelayInput(EPWM1_BASE, EPWM_DB_INPUT_EPWMA); // configure the right polarity for active high complementary config. EPWM_setDeadBandDelayPolarity(EPWM1_BASE, EPWM_DB_RED, EPWM_DB_POLARITY_ACTIVE_HIGH); EPWM_setDeadBandDelayPolarity(EPWM1_BASE, EPWM_DB_FED, EPWM_DB_POLARITY_ACTIVE_LOW); // setup the Dead-Band Rising Edge Delay Register (DBRED) EPWM_setRisingEdgeDelayCount(EPWM1_BASE, 100); // setup the Dead-Band Falling Edge Delay Register (DBFED) EPWM_setFallingEdgeDelayCount(EPWM1_BASE, 100); // setup the PWM-Chopper Control Register (PCCTL) EPWM_disableChopper(EPWM1_BASE); /* // setup the Trip Zone Select Register (TZSEL) EPWM_disableTripZoneSignals(EPWM1_BASE, EPWM_TZ_SIGNAL_CBC1 | EPWM_TZ_SIGNAL_CBC2 | EPWM_TZ_SIGNAL_CBC3 | EPWM_TZ_SIGNAL_CBC4 | EPWM_TZ_SIGNAL_CBC5 | EPWM_TZ_SIGNAL_CBC6 | EPWM_TZ_SIGNAL_DCAEVT2 | EPWM_TZ_SIGNAL_DCBEVT2 | EPWM_TZ_SIGNAL_OSHT1 | EPWM_TZ_SIGNAL_OSHT2 | EPWM_TZ_SIGNAL_OSHT3 | EPWM_TZ_SIGNAL_OSHT4 | EPWM_TZ_SIGNAL_OSHT5 | EPWM_TZ_SIGNAL_OSHT6 | EPWM_TZ_SIGNAL_DCAEVT1 | EPWM_TZ_SIGNAL_DCBEVT1); */ // EPWM_setActionQualifierT1TriggerSource(EPWM1_BASE, EPWM_AQ_TRIGGER_EVENT_TRIG_DCB_1); EPWM_setAdditionalActionQualifierActionComplete(EPWM1_BASE, EPWM_AQ_OUTPUT_A, EPWM_AQ_OUTPUT_LOW_UP_T1); EPWM_setCounterCompareValue(EPWM1_BASE, EPWM_COUNTER_COMPARE_A, 0); // // Initializing dummy values for ePWM counter and period // //EPWM_setTimeBaseCounter(EPWM1_BASE, 0); EPWM_setTimeBasePeriod(EPWM1_BASE, 2500); // // Configure ePWM1A & B to do nothing on TZA & TZB TRIP // EPWM_setTripZoneAction(EPWM1_BASE,EPWM_TZ_ACTION_EVENT_TZB, EPWM_TZ_ACTION_DISABLE); EPWM_setTripZoneAction(EPWM1_BASE,EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_DISABLE); // // Trigger event when DCBH is high // EPWM_setTripZoneDigitalCompareEventCondition(EPWM1_BASE, EPWM_TZ_DC_OUTPUT_B1, EPWM_TZ_EVENT_DCXH_HIGH); // // Configure DCBH to use TRIP4 as an input // EPWM_enableDigitalCompareTripCombinationInput(EPWM1_BASE, EPWM_DC_COMBINATIONAL_TRIPIN4, EPWM_DC_TYPE_DCBH); // // Enable DCB as OST // EPWM_enableTripZoneSignals(EPWM1_BASE, EPWM_TZ_SIGNAL_DCBEVT1); // // Configure the DCB path to be unfiltered and asynchronous // EPWM_setDigitalCompareEventSource(EPWM1_BASE, EPWM_DC_MODULE_B, EPWM_DC_EVENT_1, EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL); // // Configure TRIP4 to be CTRIP1H using the ePWM X-BAR // XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX12_CMPSS7_CTRIPH); XBAR_enableEPWMMux(XBAR_TRIP4, XBAR_MUX12); // // Clear trip flags // EPWM_clearTripZoneFlag(EPWM1_BASE, EPWM_TZ_INTERRUPT | EPWM_TZ_FLAG_OST); // // Sync the ePWM time base clock // SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC); }