This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: The problem of motor speed

Part Number: TMS320F28069M


Dear team:

One of my customers designed a motor, but with TI's FOC algorithm, he only ran the speed to 14000 rpm. Would you like to know if this motor can use FOC algorithm to increase the speed to 30000 RPM? How to operate?

Motor parameters: Voltage 310V, peak current 25A, inductance 0.2mh, back EMF 0.0085, 10 pairs of poles, maximum design speed 30000 rpm.

Best Regards