Part Number: TMS320F280041C
In user.h, in user motor parameters there is USER_MOTOR_INERTIA_Kgm2 parameter. Is this parameter only rotor inertia that is listed in a motor's datasheet or inertia of a rotor with a load attached to the rotor?
Alex
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280041C
In user.h, in user motor parameters there is USER_MOTOR_INERTIA_Kgm2 parameter. Is this parameter only rotor inertia that is listed in a motor's datasheet or inertia of a rotor with a load attached to the rotor?
Alex
It's better to use the inertia of the motor and load since you want to control the speed of the system.