I am trying to set up a low power dsp. Can you recommend it? Since there are many types of c5000 & c6000 series , it is difficult to select. The product is for Zigbee communication. We are going to choose a low power DSP to minimize battery consumption.
The chip currently used (TMS320F28377S) consumes a lot of current. normal mode: 140mA. sleep mode: 120mA.
standby mode : 110mA. halt mode: 60mA.
Specifications.
1. SPI: at least 1x
2. SCI: at least 2x.
3. ADC : at least 2x
4. CPU : 32bit
5. core : single core
6. Speed: at least 200MHz
7. Size: Smallest
8. OS : not use