Part Number: BOOSTXL-BUCKCONV
Hi,
I recently bought BOOSTXL-BUCKCONV eval kit.
The kit is not connected to any controller. It's only connected to the power supply which is providing 9V DC on JP1. The LD1 led gets ON momentarily for a sec and then remains OFF. I can see the voltage on the power supply is 9 V but the current increases to a very high value and then settles to 180mA. I expect until I don't connect any controller with a required duty cycle it should not pull any current and the LD1 led should remain ON always.
How can we debug what's going wrong?
Regards,
Vikky