Part Number: TMS320F280049
HI everybody ,
I need some EEProm on F28004x . I found libraries and examples on Gen2 : SPRAB69A – SEPTEMBER 2009 – REVISED OCTOBER 2020
is there anything dedicatedand ready to go on F28004x ? any suggestion ?
BR
Carlo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049
HI everybody ,
I need some EEProm on F28004x . I found libraries and examples on Gen2 : SPRAB69A – SEPTEMBER 2009 – REVISED OCTOBER 2020
is there anything dedicatedand ready to go on F28004x ? any suggestion ?
BR
Carlo
Carlo,
We don't have a readily available EEPROM emulation driver solution for this device.
The concept of the EEPROM emulation explained in the guide can be applied to this device as well - but the underlying flash API is different for this device as you know. One thing to note is that this device has ECC for flash - hence at least 64-bits of data has to be programmed even when the variable to update using EEPROM emulation is less than 64-bits.
Thanks and regards,
Vamsi