Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hello everyone,
Im working with the LAUNCHXL-F28379D and im currenly trying to use the SCI. Currenlly, the SCI-A is working with USB, i make a simple program to test de SCI:
This send the data throw SCI-A (USB) to a Hyperterminal, as you can see in the next image:
The problem is when i tried to look the data in the osciloscope, but, with the SCI-B (Pin 18) and SCI-C (Pin 56). In the simulink program, i only change the SCI module, from A to B or C, to conect my osciloscope an look the data but, no data is registered.
How can I configure SCI_B or SCI_C on the board, to make it work?