Other Parts Discussed in Thread: CONTROLSUITE
Hi guys.
in DSP2812, the SVPWM was initiated in register EV. The procedure is in SPRU065, pag 65/152:
http://focus.ti.com/lit/ug/spru065e/spru065e.pdf
How i do this in F28335?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CONTROLSUITE
Hi guys.
in DSP2812, the SVPWM was initiated in register EV. The procedure is in SPRU065, pag 65/152:
http://focus.ti.com/lit/ug/spru065e/spru065e.pdf
How i do this in F28335?
controlSUITE has two examples for F28335
once you install the one for PM motors will be here
C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v1.6\HVPM_Sensorless_2833x\~Docs
and the SVGEN library is
C:\ti\controlSUITE\libs\app_libs\motor_control\math_blocks\v3.0
and the PWM driver is
C:\ti\controlSUITE\libs\app_libs\motor_control\drivers\f2833x_v1.1
Jack Qian said:Where can I get the controlSUITE for 28335? Is this free ?
Thanks!
Jack,
controlSUITE is available at www.ti.com/controlsuite. Yes, it is free.
You may find this video describing the software helpful:
http://focus.ti.com/general/docs/video/Portal.tsp?entryid=0_t8vyag5y&lang=en
-Lori
Hey, i have another doubt
about what was you answer, i still studying the code C:\ti\controlSUITE\libs\app_libs\motor_control\math_blocks\v3.0\svgen_mf.c
So, i have a question. Where i put the values of variables Ta, Tb, Tc? What should registers to store the values of these variables?
HI,
In F2812, we have hardware SVPWM module , so, we need to configure appropriate for proper operation. But in F28335, doesn't have any SVPWM Module in it, so,there is no register associate to SVPWM fn..And we have to write software module / lib to generate SVPWM.
regards,
sheik
Ta, Tb, Tc are used to feed the PWM driver module.
Please see any of the FOC examples from the HV Motor Kit
C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v1.6
and please see the documentation for the two SVGEN modules (alpha/beta or magnitude/frequency)
C:\ti\controlSUITE\libs\app_libs\motor_control\math_blocks\v3.1
Hey, im back T_T
Sir, i have another doubt.
First, i took the HVACI_sensorless.c in "C:\TI\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v1.6\HVACI_Sensorless_2833x" fold. With this file, i maked a project. Then, i took all files.h and files.c in controlsuite fold and added in common fold of this project.
So, when i use the CCSv3.3, appears this:
undefined first referenced
symbol in file
--------- ----------------
_DLOG_4CH_init C:\\tidcs\\c28\\...SVPWM.obj
_DLOG_4CH_update C:\\tidcs\\c28\\...SVPWM.obj
_DeviceInit C:\\tidcs\\c28\\...SVPWM.obj
___fmax C:\\tidcs\\c28\\...SVPWM.obj
___fmin C:\\tidcs\\c28\\...SVPWM.obj
error: unresolved symbols remain
warning: entry-point symbol other than "_c_int00" specified: "code_start"
error: errors encountered during linking;
"./Debug/SVPWM.out" not built
How i fix this?
Hi Sheik,
do you have the svpwm module for F28335? can you send it to me please?
Regards
Lewis
Hi Lewis,
I am sorry I dont have any module with me right now. Simple way is to use MATLAB SIMULINK, Use Sine-wave Block and Triangular wave. Compare the point at eact intersection based on the pull the GPIO High or Low. You find lot of Literature for to generate SVPWM.
Regards
Sheik