Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi TI
I am making an SPI interface to collect data from an external ADC. The external ADC can handle up to 35 MHz clock.
I can only get out a 2 MHz clock from the SPI to get the data from the ADC. Are there any way that i can make it faster? Or should i use a EPWM module to trigger the data from the SPI, instead of a SPI- clock another time?
My problem is that i have 2 strings of 16 bit which makes it 32 bit. If i am running at 2 MHz it will still take me 16 us to get the data. I really want to make it faster so i can get the data faster.
Hope you can help me.
Regard
Asbjørn Schram Anneberg