Other Parts Discussed in Thread: C2000WARE,
HI,
I am trying to communicate two DSP launchpads f28379D so that floating data can be shared between them. As you can see in the figure below, You can see that DSP 1 carries 3 float data "vty" to DSP 2; simultaneously, the latter sends 9 ixy. Is that the launchpads have14 ADC and 6 PWM modules, but the control requires 9 + 3 +9 ADC> 14, and 9 PWM modules> 6. Therefore, I have to work with a platform made up of two DSP launchpads f28379D.
Is there a an application note where you have the to expand the number of I/O for a certain control approach? Or any suggestion I'd be grateful.