Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: LSPCLK configuration

Part Number: TMS320F28388D

Hello,

I have a question on LSPCLK configuration. Can the Low Speed Peripheral clock divider LSPCLKDIV can be configured with different values for CPU1 and CPU2? For Example: CPU1 configures LSPCLK = SYSCLK/2, but CPU2 can configure for SYSCLK/4 or so.

Or,

Is LSPCLKDIV is a common configuration and cannot be done individually from each CPUs?

Best Regards

Amulrass V

  • Hi,

    The LSPCLKDIV configuration is a part of the CLK_CFG_REGS which can be configured by either CPU1 or CPU2 based on the who owns the Clock semaphore(refer to the CLKSEM register description). For CPU2 to control this configuration, CPU2 has to first grab the semaphore by configuring the CLKSEM register. 

    Hope this helps.

    Please click on the "verify answer" button if this response has resolved your query.

    Thanks & Regards

    Pramod