Dear
I am testing AD and DA function with the controlCARD based on TMS320F28388D.
And I configure the DACB with the reference voltage “VREFHI”, I connect the pin marked as "ADCINA0" and the pin marked as"ADCINA1", which means the pin DACBOUT is connected to the pin ADCINA0.
But I found that when I set the DACB value with a digital number for example"2048" , the AD result would be 2112, when I set "3000", AD result would be "3158", And what is the root cause for this problem?
Do I need to make any additional calibration?