Hello,
customer has 2nd order filter code which produces different results (coefficients) on CPU and CLA. The CLA is not correct and the results seams a little improper like it has some rounding errors or calculating with 32bit or 64bit.
Coefficient Simulation results CPU CLA Data Type
c1 0.01241 0.0124099338 0.0125049111 float
c2 0 0.0 0. 0 float
c3 -0.01241 -0.0124099338 -0.0125049111 float
d2 1.975 1.975 1.98791492 float
d3 -0.9752 -0.975 -0.988072157 float
Would could be the reason? I can send you the code snippet per email
Regards, Holger