Other Parts Discussed in Thread: TMS320F28069F, TMS320F28027F
hello,everyone.
I use the Launchpad - 28027F and BoostXL - DRV8305EVM to drive my BLDC/PMSM motor.
and I set the #define USER_MAX_VS_MAG_PU (0.5) .
but when I use the InstaSPIN - FOC to drive my motor,but it can not reach the max speed .
I use my six step dirve my motor ,the max speed is higher than InstaSPIN - FOC .
and I test the terminal voltage scope.
I calculate the line peak voltage.
the line peak voltage is 20.137V.the dc bus voltage is 24V .
the using percent of voltage = 20.137V./24V = 84%.
but I calculate the SVPWM using percent with USER_MAX_VS_MAG_PU is equal to 0.5.
the SVPWM using percent of voltage = (2/3)*Udc*sqrt(3)/2*sqrt(3)/Udc = 100%.
but now the instaSPIN : 84%.< 100%.
and I have anather question about improving the motor max speed.
Increase the USER_MAX_VS_MAG_PU value and Field weaking all can improve the motor max speed.
I don’t know which method should I choose first .
which one is the best method to improve the motor max speed .
Thanks.