Other Parts Discussed in Thread: SFRA
I am using the SFRA with Compensation Designer matlab script to tune the 3p3z compensator. I have problem with correctly calculate the b0,b1,b2 coefficients.
In the SFRA document there is formula:
,where according to the Solar Lib document:
and to calculate nominator coefficients I should use only the part, that are with the z-1, z-2 etc... ? For example for b0:
and for b1
etc...
or multiply by the following part, that is:
I try both ways and I don't receive the correct values.
I do it at first with values generated from the Compensation Designer, to check is, the formula correctly.
I want to to adopt SFRA data into matlab script then do the tunning in Matlab with the sisotool, and then receive the Compensation transfer function, then multiply it by generated transfer function of initial model and by solver calculate the pole and zeros frequency.
I have correctly values from calculating the denominator coefficients (a1,a2...)