This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35M22C: choose

Part Number: F28M35M22C


Dear,

Request :70MHz Frequency, RAM 64KB,512KB Flash,  UART x5,I2C x 2,SPI x2 ; as above, Can you promote suitable MCU ?

  • Hi,

    If you have any project details you'd like to share, I would be more than happy to provide a more personalized recommendation and could possibly point you to reference designs as well. With the information given, I would recommend taking a look at our Concerto  family as these parts most closely match the required specs you've posted. 

    Hope this helps,

    Rick