This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: TMS320F28377D

Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE

Hi,

I am starting with programming the SPI interface with AD4112 but I can't find a code example on TI's website. Is there any similar code I can refer?

AD4112: Single Supply, 24-Bit, Sigma-Delta ADC with ±10 V and 0 mA to 20 mA Inputs

  • Hi Suraj,

    Please download our software package, C2000Ware, and our Integrated Development Environment (IDE), Code Composer Studio (CCS). 

    Once both are installed you can navigate to the following directory within C2000Ware to find examples for our SPI Module

    C:\ti\c2000\C2000Ware_version\driverlib\f2837xd\examples\cpu1\spi 

    To import the examples in CCS go to Project -> Import CCS Projects -> Navigate to the path above -> select the project.

    If you are new to C2000 or to the F28377D device then this is a great starting point:  

    Best Regards,

    Marlyn