This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: TMS320F28377S

Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE

Hi,

I have two identical CLA tasks for filtering. But in CLA task 2 I am getting error that statement is unreachable 

//
//Task 1 (C) Variables
//

    #pragma DATA_SECTION(xn1,"CpuToCla1MsgRAM")
    float xn1; //input data
    #pragma DATA_SECTION(yn1,"Cla1ToCpuMsgRAM")
    float yn1; //filtered data
    #pragma DATA_SECTION(W1,"CLADataLS0")
    float W1[FILTER_LEN] ={0.002837,0.0030005,0.0034464,0.0041735,0.005175,0.0064387,0.0079473,
                          0.0096783,0.011605,0.013696,0.015917,0.01823,0.020596,0.022973,0.025321,
                          0.027596,0.02976,0.031772,0.033597,0.035201,0.036555,0.037636,0.038421,
                          0.038899,0.039059,0.038899,0.038421,0.037636,0.036555,0.035201,0.033597,
                          0.031772,0.02976,0.027596,0.025321,0.022973,0.020596,0.01823,0.015917,
                          0.013696,0.011605,0.0096783,0.0079473,0.0064387,0.005175,0.0041735,0.0034464,
                          0.0030005,0.0028375};
    #pragma DATA_SECTION(fDelayLine1,"CLADataLS0")
    float fDelayLine1[FILTER_LEN] = {0,0,0,0,0,0,0,0,0,0,
                                    0,0,0,0,0,0,0,0,0,0,
                                    0,0,0,0,0,0,0,0,0,0,
                                    0,0,0,0,0,0,0,0,0,0,
                                    0,0,0,0,0,0,0,0,0,};



//
//Task 2 (C) Variables
//
#pragma DATA_SECTION(xn2,"CpuToCla1MsgRAM")
float xn2; //input data
#pragma DATA_SECTION(yn2,"Cla1ToCpuMsgRAM")
float yn2; //filtered data
#pragma DATA_SECTION(W2,"CLADataLS0")
float W2[FILTER_LEN] ={0.002837,0.0030005,0.0034464,0.0041735,0.005175,0.0064387,0.0079473,
                      0.0096783,0.011605,0.013696,0.015917,0.01823,0.020596,0.022973,0.025321,
                      0.027596,0.02976,0.031772,0.033597,0.035201,0.036555,0.037636,0.038421,
                      0.038899,0.039059,0.038899,0.038421,0.037636,0.036555,0.035201,0.033597,
                      0.031772,0.02976,0.027596,0.025321,0.022973,0.020596,0.01823,0.015917,
                      0.013696,0.011605,0.0096783,0.0079473,0.0064387,0.005175,0.0041735,0.0034464,
                      0.0030005,0.0028375};
#pragma DATA_SECTION(fDelayLine2,"CLADataLS0")
float fDelayLine2[FILTER_LEN] = {0,0,0,0,0,0,0,0,0,0,
                                0,0,0,0,0,0,0,0,0,0,
                                0,0,0,0,0,0,0,0,0,0,
                                0,0,0,0,0,0,0,0,0,0,
                                0,0,0,0,0,0,0,0,0,};

thanks vadim

  • Vadim,

    I don't see anything obvious from the screenshot.  Can you provide the following:

    1. Preprocessed source file
    2. Compiler Version
    3. Compiler Options Used

    Refer to this page for how to create (1).

    http://software-dl.ti.com/ccs/esd/documents/sdto_cgt_How-to-Submit-a-Compiler-Test-Case.html

    Regards

    Lori

  • Building file: "../__FilterFIR_loop.c"
    Invoking: C2000 Compiler
    "C:/ti/ccs1011/ccs/tools/compiler/ti-cgt-c2000_20.2.4.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 --include_path="C:/ti/ccs1011/ccs/tools/compiler/ti-cgt-c2000_20.2.4.LTS/include" --include_path="C:/ti/C2000Ware_3_03_00_00_Software/device_support/f2837xs/headers/include" --include_path="C:/ti/C2000Ware_3_03_00_00_Software/device_support/f2837xs/common/include" --include_path="C:/ti/C2000Ware_3_03_00_00_Software/device_support/f2837xs/examples/cpu1/cla_iir2p2z/cpu01/" --define=_LAUNCHXL_F28377S --define=CPU_FRQ_200MHZ --define=CPU1 -g --preproc_with_comment --preproc_with_compile --diag_suppress=10068 --diag_warning=225 --display_error_number --abi=coffabi --cla_support=cla1 "../__FilterFIR_loop.c"
    Finished building: "../__FilterFIR_loop.c"

    Building file: "../_FilterFIR_loop.cla"
    Invoking: C2000 Compiler
    "C:/ti/ccs1011/ccs/tools/compiler/ti-cgt-c2000_20.2.4.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 --include_path="C:/ti/ccs1011/ccs/tools/compiler/ti-cgt-c2000_20.2.4.LTS/include" --include_path="C:/ti/C2000Ware_3_03_00_00_Software/device_support/f2837xs/headers/include" --include_path="C:/ti/C2000Ware_3_03_00_00_Software/device_support/f2837xs/common/include" --include_path="C:/ti/C2000Ware_3_03_00_00_Software/device_support/f2837xs/examples/cpu1/cla_iir2p2z/cpu01/" --define=_LAUNCHXL_F28377S --define=CPU_FRQ_200MHZ --define=CPU1 -g --preproc_with_comment --preproc_with_compile --diag_suppress=10068 --diag_warning=225 --display_error_number --abi=coffabi --cla_support=cla1 "../_FilterFIR_loop.cla"
    "../_FilterFIR_loop.cla", line 36: warning #112-D: statement is unreachable
    Finished building: "../_FilterFIR_loop.cla"

    __FilterFIR_loop.pp.txt

    //
    //#############################################################################
    //
    // FILE:   cla_fir32_shared.h
    //
    // TITLE:  CLA 5 Tap FIR filter
    //
    //#############################################################################
    // $TI Release: F2837xS Support Library v3.11.00.00 $
    // $Release Date: Sun Oct  4 15:58:38 IST 2020 $
    // $Copyright:
    // Copyright (C) 2014-2020 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //#############################################################################
    
    //
    // Included Files
    //
    //###########################################################################
    //
    // FILE:   F2837xS_Cla_defines.h
    //
    // TITLE:  #defines used in CLA examples
    //
    //###########################################################################
    // $TI Release: F2837xS Support Library v3.11.00.00 $
    // $Release Date: Sun Oct  4 15:58:38 IST 2020 $
    // $Copyright:
    // Copyright (C) 2014-2020 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without 
    // modification, are permitted provided that the following conditions 
    // are met:
    // 
    //   Redistributions of source code must retain the above copyright 
    //   notice, this list of conditions and the following disclaimer.
    // 
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the 
    //   documentation and/or other materials provided with the   
    //   distribution.
    // 
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    // 
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    
    
    
    //
    // Defines
    //
    
    //
    // MCTL Register
    //
    
    //
    // MMEMCFG Register
    //
    
    //
    // MIER Interrupt Enable Register
    //
    
    //
    // Peripheral Interrupt Source Select define for DMAnCLASourceSelect Register
    //
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    
    //
    // End of file
    //
    /*****************************************************************************/
    /* STDINT.H                                                                  */
    /*                                                                           */
    /* Copyright (c) 2002 Texas Instruments Incorporated                         */
    /* http://www.ti.com/                                                        */
    /*                                                                           */
    /*  Redistribution and  use in source  and binary forms, with  or without    */
    /*  modification,  are permitted provided  that the  following conditions    */
    /*  are met:                                                                 */
    /*                                                                           */
    /*     Redistributions  of source  code must  retain the  above copyright    */
    /*     notice, this list of conditions and the following disclaimer.         */
    /*                                                                           */
    /*     Redistributions in binary form  must reproduce the above copyright    */
    /*     notice, this  list of conditions  and the following  disclaimer in    */
    /*     the  documentation  and/or   other  materials  provided  with  the    */
    /*     distribution.                                                         */
    /*                                                                           */
    /*     Neither the  name of Texas Instruments Incorporated  nor the names    */
    /*     of its  contributors may  be used to  endorse or  promote products    */
    /*     derived  from   this  software  without   specific  prior  written    */
    /*     permission.                                                           */
    /*                                                                           */
    /*  THIS SOFTWARE  IS PROVIDED BY THE COPYRIGHT  HOLDERS AND CONTRIBUTORS    */
    /*  "AS IS"  AND ANY  EXPRESS OR IMPLIED  WARRANTIES, INCLUDING,  BUT NOT    */
    /*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR    */
    /*  A PARTICULAR PURPOSE ARE DISCLAIMED.  IN NO EVENT SHALL THE COPYRIGHT    */
    /*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,    */
    /*  SPECIAL,  EXEMPLARY,  OR CONSEQUENTIAL  DAMAGES  (INCLUDING, BUT  NOT    */
    /*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,    */
    /*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY    */
    /*  THEORY OF  LIABILITY, WHETHER IN CONTRACT, STRICT  LIABILITY, OR TORT    */
    /*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE    */
    /*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.     */
    /*                                                                           */
    /*****************************************************************************/
    
    /*****************************************************************************/
    /* _ti_config.h                                                              */
    /*                                                                           */
    /* Copyright (c) 2017 Texas Instruments Incorporated                         */
    /* http://www.ti.com/                                                        */
    /*                                                                           */
    /*  Redistribution and  use in source  and binary forms, with  or without    */
    /*  modification,  are permitted provided  that the  following conditions    */
    /*  are met:                                                                 */
    /*                                                                           */
    /*     Redistributions  of source  code must  retain the  above copyright    */
    /*     notice, this list of conditions and the following disclaimer.         */
    /*                                                                           */
    /*     Redistributions in binary form  must reproduce the above copyright    */
    /*     notice, this  list of conditions  and the following  disclaimer in    */
    /*     the  documentation  and/or   other  materials  provided  with  the    */
    /*     distribution.                                                         */
    /*                                                                           */
    /*     Neither the  name of Texas Instruments Incorporated  nor the names    */
    /*     of its  contributors may  be used to  endorse or  promote products    */
    /*     derived  from   this  software  without   specific  prior  written    */
    /*     permission.                                                           */
    /*                                                                           */
    /*  THIS SOFTWARE  IS PROVIDED BY THE COPYRIGHT  HOLDERS AND CONTRIBUTORS    */
    /*  "AS IS"  AND ANY  EXPRESS OR IMPLIED  WARRANTIES, INCLUDING,  BUT NOT    */
    /*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR    */
    /*  A PARTICULAR PURPOSE ARE DISCLAIMED.  IN NO EVENT SHALL THE COPYRIGHT    */
    /*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,    */
    /*  SPECIAL,  EXEMPLARY,  OR CONSEQUENTIAL  DAMAGES  (INCLUDING, BUT  NOT    */
    /*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,    */
    /*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY    */
    /*  THEORY OF  LIABILITY, WHETHER IN CONTRACT, STRICT  LIABILITY, OR TORT    */
    /*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE    */
    /*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.     */
    /*                                                                           */
    /*****************************************************************************/
    
    
    /*Unsupported pragmas are omitted */
    # pragma diag_push
    # pragma CHECK_MISRA("-19.7")
    # pragma CHECK_MISRA("-19.4")
    # pragma CHECK_MISRA("-19.1")
    # pragma CHECK_MISRA("-19.15")
    # pragma diag_pop
    
    _Pragma("diag_push")
    _Pragma("CHECK_MISRA(\"-19.4\")")
    _Pragma("CHECK_MISRA(\"-19.1\")")
    _Pragma("CHECK_MISRA(\"-19.6\")")
    
    /* Hide uses of the TI proprietary macros behind other macros.
        Implementations that don't implement these features should leave
        these macros undefined. */
    
    
    
    /* Common definitions */
    
    /* C */
     /* C89/C99 */
    
    
    
    
    
    /* _TI_NOEXCEPT_CPP14 is defined to noexcept only when compiling for C++14. It
       is intended to be used for functions like abort and atexit that are supposed
       to be declared noexcept only in C++14 mode. */
    
    
    
    /* Target-specific definitions */
    /*****************************************************************************/
    /* linkage.h                                                                  */
    /*                                                                           */
    /* Copyright (c) 1998 Texas Instruments Incorporated                         */
    /* http://www.ti.com/                                                        */
    /*                                                                           */
    /*  Redistribution and  use in source  and binary forms, with  or without    */
    /*  modification,  are permitted provided  that the  following conditions    */
    /*  are met:                                                                 */
    /*                                                                           */
    /*     Redistributions  of source  code must  retain the  above copyright    */
    /*     notice, this list of conditions and the following disclaimer.         */
    /*                                                                           */
    /*     Redistributions in binary form  must reproduce the above copyright    */
    /*     notice, this  list of conditions  and the following  disclaimer in    */
    /*     the  documentation  and/or   other  materials  provided  with  the    */
    /*     distribution.                                                         */
    /*                                                                           */
    /*     Neither the  name of Texas Instruments Incorporated  nor the names    */
    /*     of its  contributors may  be used to  endorse or  promote products    */
    /*     derived  from   this  software  without   specific  prior  written    */
    /*     permission.                                                           */
    /*                                                                           */
    /*  THIS SOFTWARE  IS PROVIDED BY THE COPYRIGHT  HOLDERS AND CONTRIBUTORS    */
    /*  "AS IS"  AND ANY  EXPRESS OR IMPLIED  WARRANTIES, INCLUDING,  BUT NOT    */
    /*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR    */
    /*  A PARTICULAR PURPOSE ARE DISCLAIMED.  IN NO EVENT SHALL THE COPYRIGHT    */
    /*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,    */
    /*  SPECIAL,  EXEMPLARY,  OR CONSEQUENTIAL  DAMAGES  (INCLUDING, BUT  NOT    */
    /*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,    */
    /*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY    */
    /*  THEORY OF  LIABILITY, WHETHER IN CONTRACT, STRICT  LIABILITY, OR TORT    */
    /*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE    */
    /*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.     */
    /*                                                                           */
    /*****************************************************************************/
    
    
    #pragma diag_push
    #pragma CHECK_MISRA("-19.4") /* macros required for implementation */
    
    /* No modifiers needed to access code */
    
    
    /*--------------------------------------------------------------------------*/
    /* Define _DATA_ACCESS ==> how to access RTS global or static data          */
    /*--------------------------------------------------------------------------*/
    
    /*--------------------------------------------------------------------------*/
    /* Define _OPTIMIZE_FOR_SPACE ==> Always optimize for space.                */
    /*--------------------------------------------------------------------------*/
    
    /*--------------------------------------------------------------------------*/
    /* Define _IDECL ==> how inline functions are declared                      */
    /*--------------------------------------------------------------------------*/
    
    #pragma diag_pop
    
    
    _Pragma("diag_pop")
    
    
    _Pragma("diag_push")
    _Pragma("CHECK_MISRA(\"-19.1\")") /* no code before #include */
    _Pragma("CHECK_MISRA(\"-19.7\")") /* prefer functions to macros */
    
    /*****************************************************************************/
    /* _STDINT40.H                                                               */
    /*                                                                           */
    /* Copyright (c) 2018 Texas Instruments Incorporated                         */
    /* http://www.ti.com/                                                        */
    /*                                                                           */
    /*  Redistribution and  use in source  and binary forms, with  or without    */
    /*  modification,  are permitted provided  that the  following conditions    */
    /*  are met:                                                                 */
    /*                                                                           */
    /*     Redistributions  of source  code must  retain the  above copyright    */
    /*     notice, this list of conditions and the following disclaimer.         */
    /*                                                                           */
    /*     Redistributions in binary form  must reproduce the above copyright    */
    /*     notice, this  list of conditions  and the following  disclaimer in    */
    /*     the  documentation  and/or   other  materials  provided  with  the    */
    /*     distribution.                                                         */
    /*                                                                           */
    /*     Neither the  name of Texas Instruments Incorporated  nor the names    */
    /*     of its  contributors may  be used to  endorse or  promote products    */
    /*     derived  from   this  software  without   specific  prior  written    */
    /*     permission.                                                           */
    /*                                                                           */
    /*  THIS SOFTWARE  IS PROVIDED BY THE COPYRIGHT  HOLDERS AND CONTRIBUTORS    */
    /*  "AS IS"  AND ANY  EXPRESS OR IMPLIED  WARRANTIES, INCLUDING,  BUT NOT    */
    /*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR    */
    /*  A PARTICULAR PURPOSE ARE DISCLAIMED.  IN NO EVENT SHALL THE COPYRIGHT    */
    /*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,    */
    /*  SPECIAL,  EXEMPLARY,  OR CONSEQUENTIAL  DAMAGES  (INCLUDING, BUT  NOT    */
    /*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,    */
    /*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY    */
    /*  THEORY OF  LIABILITY, WHETHER IN CONTRACT, STRICT  LIABILITY, OR TORT    */
    /*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE    */
    /*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.     */
    /*                                                                           */
    /*****************************************************************************/
    
    _Pragma("diag_push")
    _Pragma("CHECK_MISRA(\"-19.7\")") /* prefer functions to macros */
    
    
    /*
       According to footnotes in the 1999 C standard, "C++ implementations
       should define these macros only when __STDC_LIMIT_MACROS is defined
       before <stdint.h> is included."
    */
    
    
    
    _Pragma("diag_pop")
    
    /*-
     * SPDX-License-Identifier: BSD-2-Clause-FreeBSD
     *
     * Copyright (c) 2001 Mike Barcroft <mike@FreeBSD.org>
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     * 1. Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     * 2. Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * THIS SOFTWARE IS PROVIDED BY THE AUTHOR AND CONTRIBUTORS ``AS IS'' AND
     * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
     * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
     * ARE DISCLAIMED.  IN NO EVENT SHALL THE AUTHOR OR CONTRIBUTORS BE LIABLE
     * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
     * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS
     * OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
     * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
     * LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY
     * OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
     * SUCH DAMAGE.
     *
     * $FreeBSD$
     */
    
    
    
    /*-
     * SPDX-License-Identifier: BSD-3-Clause
     *
     * Copyright (c) 1991, 1993
     *	The Regents of the University of California.  All rights reserved.
     *
     * This code is derived from software contributed to Berkeley by
     * Berkeley Software Design, Inc.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     * 1. Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     * 2. Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     * 3. Neither the name of the University nor the names of its contributors
     *    may be used to endorse or promote products derived from this software
     *    without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE REGENTS AND CONTRIBUTORS ``AS IS'' AND
     * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
     * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
     * ARE DISCLAIMED.  IN NO EVENT SHALL THE REGENTS OR CONTRIBUTORS BE LIABLE
     * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
     * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS
     * OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
     * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
     * LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY
     * OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
     * SUCH DAMAGE.
     *
     *	@(#)cdefs.h	8.8 (Berkeley) 1/9/95
     * $FreeBSD$
     */
    
    
    
    _Pragma("diag_push")
    _Pragma("CHECK_MISRA(\"none\")")
    
    /*
     * Testing against Clang-specific extensions.
     */
    
    
    /*
     * This code has been put in place to help reduce the addition of
     * compiler specific defines in FreeBSD code.  It helps to aid in
     * having a compiler-agnostic source tree.
     */
    
    
    
    
    
    
    
    /*
     * Macro to test if we're using a specific version of gcc or later.
     */
    
    /*
     * The __CONCAT macro is used to concatenate parts of symbol names, e.g.
     * with "#define OLD(foo) __CONCAT(old,foo)", OLD(foo) produces oldfoo.
     * The __CONCAT macro is a bit tricky to use if it must work in non-ANSI
     * mode -- there must be no spaces between its arguments, and for nested
     * __CONCAT's, all the __CONCAT's must be at the left.  __CONCAT can also
     * concatenate double-quoted strings produced by the __STRING macro, but
     * this only works with ANSI C.
     *
     * __XSTRING is like __STRING, but it expands any macros in its argument
     * first.  It is only available with ANSI C.
     */
    
    
    
    /*
     * Compiler-dependent macros to help declare dead (non-returning) and
     * pure (no side effects) functions, and unused variables.  They are
     * null except for versions of gcc that are known to support the features
     * properly (old versions of gcc-2 supported the dead and pure features
     * in a different (wrong) way).  If we do not provide an implementation
     * for a given compiler, let the compile fail if it is told to use
     * a feature that we cannot live without.
     */
    
    /*
     * TI ADD - check that __GNUC__ is defined before referencing it to avoid
     *          generating an error when __GNUC__ treated as zero warning is
     *          promoted to an error via -pdse195 option.
     */
    
    
    
    /*
     * Keywords added in C11.
     */
    
    
    
    
    /*
     * No native support for _Atomic(). Place object in structure to prevent
     * most forms of direct non-atomic access.
     */
    
    
    
    /*
     * XXX: Some compilers (Clang 3.3, GCC 4.7) falsely announce C++11 mode
     * without actually supporting the thread_local keyword. Don't check for
     * the presence of C++11 when defining _Thread_local.
     */
    
    
    /*
     * Emulation of C11 _Generic().  Unlike the previously defined C11
     * keywords, it is not possible to implement this using exactly the same
     * syntax.  Therefore implement something similar under the name
     * __generic().  Unlike _Generic(), this macro can only distinguish
     * between a single type, so it requires nested invocations to
     * distinguish multiple cases.
     */
    
    
    /*
     * C99 Static array indices in function parameter declarations.  Syntax such as:
     * void bar(int myArray[static 10]);
     * is allowed in C99 but not in C++.  Define __min_size appropriately so
     * headers using it can be compiled in either language.  Use like this:
     * void bar(int myArray[__min_size(10)]);
     */
    
    
    
    
    
    
    
    /* XXX: should use `#if __STDC_VERSION__ < 199901'. */
    
    
    /* C++11 exposes a load of C99 stuff */
    
    /*
     * GCC 2.95 provides `__restrict' as an extension to C90 to support the
     * C99-specific `restrict' type qualifier.  We happen to use `__restrict' as
     * a way to define the `restrict' type qualifier without disturbing older
     * software that is unaware of C99 keywords.
     * The TI compiler supports __restrict in all compilation modes.
     */
    
    /*
     * GNU C version 2.96 adds explicit branch prediction so that
     * the CPU back-end can hint the processor and also so that
     * code blocks can be reordered such that the predicted path
     * sees a more linear flow, thus improving cache behavior, etc.
     *
     * The following two macros provide us with a way to utilize this
     * compiler feature.  Use __predict_true() if you expect the expression
     * to evaluate to true, and __predict_false() if you expect the
     * expression to evaluate to false.
     *
     * A few notes about usage:
     *
     *	* Generally, __predict_false() error condition checks (unless
     *	  you have some _strong_ reason to do otherwise, in which case
     *	  document it), and/or __predict_true() `no-error' condition
     *	  checks, assuming you want to optimize for the no-error case.
     *
     *	* Other than that, if you don't know the likelihood of a test
     *	  succeeding from empirical or other `hard' evidence, don't
     *	  make predictions.
     *
     *	* These are meant to be used in places that are run `a lot'.
     *	  It is wasteful to make predictions in code that is run
     *	  seldomly (e.g. at subsystem initialization time) as the
     *	  basic block reordering that this affects can often generate
     *	  larger code.
     */
    
    
    /*
     * We define this here since <stddef.h>, <sys/queue.h>, and <sys/types.h>
     * require it.
     */
    
    /*
     * Given the pointer x to the member m of the struct s, return
     * a pointer to the containing structure.  When using GCC, we first
     * assign pointer x to a local variable, to check that its type is
     * compatible with member m.
     */
    
    /*
     * Compiler-dependent macros to declare that functions take printf-like
     * or scanf-like arguments.  They are null except for versions of gcc
     * that are known to support the features properly (old versions of gcc-2
     * didn't permit keeping the keywords out of the application namespace).
     */
    
    /* Compiler-dependent macros that rely on FreeBSD-specific extensions. */
    
    
    
    /*
     * The following definition might not work well if used in header files,
     * but it should be better than nothing.  If you want a "do nothing"
     * version, then it should generate some harmless declaration, such as:
     *    #define	__IDSTRING(name,string)	struct __hack
     */
    
    
    /*
     * Embed the rcs id of a source file in the resulting library.  Note that in
     * more recent ELF binutils, we use .ident allowing the ID to be stripped.
     * Usage:
     *	__FBSDID("$FreeBSD$");
     */
    
    
    
    
    
    
    
    
    /*-
     * The following definitions are an extension of the behavior originally
     * implemented in <sys/_posix.h>, but with a different level of granularity.
     * POSIX.1 requires that the macros we test be defined before any standard
     * header file is included.
     *
     * Here's a quick run-down of the versions:
     *  defined(_POSIX_SOURCE)		1003.1-1988
     *  _POSIX_C_SOURCE == 1		1003.1-1990
     *  _POSIX_C_SOURCE == 2		1003.2-1992 C Language Binding Option
     *  _POSIX_C_SOURCE == 199309		1003.1b-1993
     *  _POSIX_C_SOURCE == 199506		1003.1c-1995, 1003.1i-1995,
     *					and the omnibus ISO/IEC 9945-1: 1996
     *  _POSIX_C_SOURCE == 200112		1003.1-2001
     *  _POSIX_C_SOURCE == 200809		1003.1-2008
     *
     * In addition, the X/Open Portability Guide, which is now the Single UNIX
     * Specification, defines a feature-test macro which indicates the version of
     * that specification, and which subsumes _POSIX_C_SOURCE.
     *
     * Our macros begin with two underscores to avoid namespace screwage.
     */
    
    /* Deal with IEEE Std. 1003.1-1990, in which _POSIX_C_SOURCE == 1. */
    
    /* Deal with IEEE Std. 1003.2-1992, in which _POSIX_C_SOURCE == 2. */
    
    /* Deal with various X/Open Portability Guides and Single UNIX Spec. */
    
    /*
     * Deal with all versions of POSIX.  The ordering relative to the tests above is
     * important.
     */
    /*-
     * Deal with _ANSI_SOURCE:
     * If it is defined, and no other compilation environment is explicitly
     * requested, then define our internal feature-test macros to zero.  This
     * makes no difference to the preprocessor (undefined symbols in preprocessing
     * expressions are defined to have value zero), but makes it more convenient for
     * a test program to print out the values.
     *
     * If a program mistakenly defines _ANSI_SOURCE and some other macro such as
     * _POSIX_C_SOURCE, we will assume that it wants the broader compilation
     * environment (and in fact we will never get here).
     */
    
    /* User override __EXT1_VISIBLE */
    
    
    /*
     * Old versions of GCC use non-standard ARM arch symbols; acle-compat.h
     * translates them to __ARM_ARCH and the modern feature symbols defined by ARM.
     */
    
    /*
     * Nullability qualifiers: currently only supported by Clang.
     */
    
    /*
     * Type Safety Checking
     *
     * Clang provides additional attributes to enable checking type safety
     * properties that cannot be enforced by the C type system. 
     */
    
    
    /*
     * Lock annotations.
     *
     * Clang provides support for doing basic thread-safety tests at
     * compile-time, by marking which locks will/should be held when
     * entering/leaving a functions.
     *
     * Furthermore, it is also possible to annotate variables and structure
     * members to enforce that they are only accessed when certain locks are
     * held.
     */
    
    
    /* Structure implements a lock. */
    
    /* Function acquires an exclusive or shared lock. */
    
    /* Function attempts to acquire an exclusive or shared lock. */
    
    /* Function releases a lock. */
    
    /* Function asserts that an exclusive or shared lock is held. */
    
    /* Function requires that an exclusive or shared lock is or is not held. */
    
    /* Function should not be analyzed. */
    
    /* Guard variables and structure members by lock. */
    
    _Pragma("diag_pop")
    
    /*-
     * SPDX-License-Identifier: BSD-2-Clause-FreeBSD
     *
     * Copyright (c) 2002 Mike Barcroft <mike@FreeBSD.org>
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     * 1. Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     * 2. Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * THIS SOFTWARE IS PROVIDED BY THE AUTHOR AND CONTRIBUTORS ``AS IS'' AND
     * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
     * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
     * ARE DISCLAIMED.  IN NO EVENT SHALL THE AUTHOR OR CONTRIBUTORS BE LIABLE
     * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
     * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS
     * OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
     * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
     * LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY
     * OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
     * SUCH DAMAGE.
     *
     * $FreeBSD$
     */
    
    
    /*****************************************************************************/
    /*  _TYPES.H                                                                 */
    /*                                                                           */
    /* Copyright (c) 2017 Texas Instruments Incorporated                         */
    /* http://www.ti.com/                                                        */
    /*                                                                           */
    /*  Redistribution and  use in source  and binary forms, with  or without    */
    /*  modification,  are permitted provided  that the  following conditions    */
    /*  are met:                                                                 */
    /*                                                                           */
    /*     Redistributions  of source  code must  retain the  above copyright    */
    /*     notice, this list of conditions and the following disclaimer.         */
    /*                                                                           */
    /*     Redistributions in binary form  must reproduce the above copyright    */
    /*     notice, this  list of conditions  and the following  disclaimer in    */
    /*     the  documentation  and/or   other  materials  provided  with  the    */
    /*     distribution.                                                         */
    /*                                                                           */
    /*     Neither the  name of Texas Instruments Incorporated  nor the names    */
    /*     of its  contributors may  be used to  endorse or  promote products    */
    /*     derived  from   this  software  without   specific  prior  written    */
    /*     permission.                                                           */
    /*                                                                           */
    /*  THIS SOFTWARE  IS PROVIDED BY THE COPYRIGHT  HOLDERS AND CONTRIBUTORS    */
    /*  "AS IS"  AND ANY  EXPRESS OR IMPLIED  WARRANTIES, INCLUDING,  BUT NOT    */
    /*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR    */
    /*  A PARTICULAR PURPOSE ARE DISCLAIMED.  IN NO EVENT SHALL THE COPYRIGHT    */
    /*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,    */
    /*  SPECIAL,  EXEMPLARY,  OR CONSEQUENTIAL  DAMAGES  (INCLUDING, BUT  NOT    */
    /*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,    */
    /*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY    */
    /*  THEORY OF  LIABILITY, WHETHER IN CONTRACT, STRICT  LIABILITY, OR TORT    */
    /*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE    */
    /*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.     */
    /*                                                                           */
    /*****************************************************************************/
    
    
    
    #pragma diag_push
    /* This file is required to use base types */
    #pragma CHECK_MISRA("-6.3")
    
    
    /*
     * Basic types upon which most other types are built.
     */
        typedef          short  __int16_t;
        typedef unsigned short __uint16_t;
        typedef          int    __int32_t;
        typedef unsigned int   __uint32_t;
    
    
    /* LONGLONG */
    typedef	long long		__int64_t;
    
    /* LONGLONG */
    typedef	unsigned long long	__uint64_t;
    
    /*
     * Standard type definitions.
     */
    typedef	__uint32_t	__clock_t;		/* clock()... */
    typedef	__int32_t	__critical_t;
    typedef	double		__double_t;
    typedef	float		__float_t;
    typedef	__int32_t	__intfptr_t;
    typedef	__int64_t	__intmax_t;
    typedef	__int16_t	__intptr_t;
    
    typedef	__int16_t	__int_fast8_t;
    typedef	__int16_t	__int_fast16_t;
    typedef	__int32_t	__int_fast32_t;
    typedef	__int64_t	__int_fast64_t;
    typedef	__int16_t	__int_least8_t;
    typedef	__int16_t	__int_least16_t;
    typedef	__int32_t	__int_least32_t;
    typedef	__int64_t	__int_least64_t;
    typedef	int __ptrdiff_t;		/* ptr1 - ptr2 */
    typedef	__int16_t	__register_t;
    typedef	__int32_t	__segsz_t;		/* segment size (in pages) */
    typedef	unsigned int	__size_t;		/* sizeof() */
    typedef	__int32_t	__ssize_t;		/* byte count or error */
    typedef __uint32_t      __time_t;
    typedef	__uint32_t	__uintfptr_t;
    typedef	__uint64_t	__uintmax_t;
    typedef	__uint16_t	__uintptr_t;
    
    typedef	__uint16_t	__uint_fast8_t;
    typedef	__uint16_t	__uint_fast16_t;
    typedef	__uint32_t	__uint_fast32_t;
    typedef	__uint64_t	__uint_fast64_t;
    typedef	__uint16_t	__uint_least8_t;
    typedef	__uint16_t	__uint_least16_t;
    typedef	__uint32_t	__uint_least32_t;
    typedef	__uint64_t	__uint_least64_t;
    typedef	__uint16_t	__u_register_t;
    typedef	__uint32_t	__vm_offset_t;
    typedef	__uint32_t	__vm_paddr_t;
    typedef	__uint32_t	__vm_size_t;
    
    typedef	unsigned short ___wchar_t;
    
    
    /*
     * POSIX target specific _off_t type definition
     */
    typedef long int _off_t;
    
    /*
     * Unusual type definitions.
     */
    typedef char* __va_list;
    
    #pragma diag_pop
    
    
    _Pragma("diag_push")
    /* This file is required to use types without size and signedness */
    _Pragma("CHECK_MISRA(\"-6.3\")")
    
    /*
     * Standard type definitions.
     */
    typedef	__int32_t	__blksize_t;	/* file block size */
    typedef	__int64_t	__blkcnt_t;	/* file block count */
    typedef	__int32_t	__clockid_t;	/* clock_gettime()... */
    typedef	__uint32_t	__fflags_t;	/* file flags */
    typedef	__uint64_t	__fsblkcnt_t;
    typedef	__uint64_t	__fsfilcnt_t;
    typedef	__uint32_t	__gid_t;
    typedef	__int64_t	__id_t;		/* can hold a gid_t, pid_t, or uid_t */
    typedef	__uint64_t	__ino_t;	/* inode number */
    typedef	long		__key_t;	/* IPC key (for Sys V IPC) */
    typedef	__int32_t	__lwpid_t;	/* Thread ID (a.k.a. LWP) */
    typedef	__uint16_t	__mode_t;	/* permissions */
    typedef	int		__accmode_t;	/* access permissions */
    typedef	int		__nl_item;
    typedef	__uint64_t	__nlink_t;	/* link count */
    typedef	_off_t	        __off_t;	/* file offset (target-specific)  */
    typedef	__int64_t	__off64_t;	/* file offset (always 64-bit)    */
    typedef	__int32_t	__pid_t;	/* process [group] */
    typedef	__int64_t	__rlim_t;	/* resource limit - intentionally */
    					/* signed, because of legacy code */
    					/* that uses -1 for RLIM_INFINITY */
    typedef	__uint16_t	__sa_family_t;
    typedef	__uint32_t	__socklen_t;
    typedef	long		__suseconds_t;	/* microseconds (signed) */
    typedef	struct __timer	*__timer_t;	/* timer_gettime()... */
    typedef	struct __mq	*__mqd_t;	/* mq_open()... */
    typedef	__uint32_t	__uid_t;
    typedef	unsigned int	__useconds_t;	/* microseconds (unsigned) */
    typedef	int		__cpuwhich_t;	/* which parameter for cpuset. */
    typedef	int		__cpulevel_t;	/* level parameter for cpuset. */
    typedef int		__cpusetid_t;	/* cpuset identifier. */
    
    /*
     * Unusual type definitions.
     */
    /*
     * rune_t is declared to be an ``int'' instead of the more natural
     * ``unsigned long'' or ``long''.  Two things are happening here.  It is not
     * unsigned so that EOF (-1) can be naturally assigned to it and used.  Also,
     * it looks like 10646 will be a 31 bit standard.  This means that if your
     * ints cannot hold 32 bits, you will be in trouble.  The reason an int was
     * chosen over a long is that the is*() and to*() routines take ints (says
     * ANSI C), but they use __ct_rune_t instead of int.
     *
     * NOTE: rune_t is not covered by ANSI nor other standards, and should not
     * be instantiated outside of lib/libc/locale.  Use wchar_t.  wint_t and
     * rune_t must be the same type.  Also, wint_t should be able to hold all
     * members of the largest character set plus one extra value (WEOF), and
     * must be at least 16 bits.
     */
    typedef	int		__ct_rune_t;	/* arg type for ctype funcs */
    
    typedef	__ct_rune_t	__rune_t;	/* rune_t (see above) */
    typedef	__ct_rune_t	__wint_t;	/* wint_t (see above) */
    
    /* Clang already provides these types as built-ins, but only in C++ mode. */
    typedef	__uint_least16_t __char16_t;
    typedef	__uint_least32_t __char32_t;
    /* In C++11, char16_t and char32_t are built-in types. */
    
    typedef struct {
    	long long __max_align1 __attribute__((aligned(__alignof__(long long))));
    	long double __max_align2 __attribute__((aligned(__alignof__(long double))));
    } __max_align_t;
    
    typedef	__uint64_t	__dev_t;	/* device number */
    
    typedef	__uint32_t	__fixpt_t;	/* fixed point number */
    
    /*
     * mbstate_t is an opaque object to keep conversion state during multibyte
     * stream conversions.
     */
    
    typedef int _Mbstatet;
    
    typedef _Mbstatet __mbstate_t;
    
    typedef __uintmax_t     __rman_res_t;
    
    /*
     * When the following macro is defined, the system uses 64-bit inode numbers.
     * Programs can use this to avoid including <sys/param.h>, with its associated
     * namespace pollution.
     */
    
    _Pragma("diag_pop")
    
    
    /*****************************************************************************/
    /*  _STDINT.H                                                                */
    /*                                                                           */
    /* Copyright (c) 2019 Texas Instruments Incorporated                         */
    /* http://www.ti.com/                                                        */
    /*                                                                           */
    /*  Redistribution and  use in source  and binary forms, with  or without    */
    /*  modification,  are permitted provided  that the  following conditions    */
    /*  are met:                                                                 */
    /*                                                                           */
    /*     Redistributions  of source  code must  retain the  above copyright    */
    /*     notice, this list of conditions and the following disclaimer.         */
    /*                                                                           */
    /*     Redistributions in binary form  must reproduce the above copyright    */
    /*     notice, this  list of conditions  and the following  disclaimer in    */
    /*     the  documentation  and/or   other  materials  provided  with  the    */
    /*     distribution.                                                         */
    /*                                                                           */
    /*     Neither the  name of Texas Instruments Incorporated  nor the names    */
    /*     of its  contributors may  be used to  endorse or  promote products    */
    /*     derived  from   this  software  without   specific  prior  written    */
    /*     permission.                                                           */
    /*                                                                           */
    /*  THIS SOFTWARE  IS PROVIDED BY THE COPYRIGHT  HOLDERS AND CONTRIBUTORS    */
    /*  "AS IS"  AND ANY  EXPRESS OR IMPLIED  WARRANTIES, INCLUDING,  BUT NOT    */
    /*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR    */
    /*  A PARTICULAR PURPOSE ARE DISCLAIMED.  IN NO EVENT SHALL THE COPYRIGHT    */
    /*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,    */
    /*  SPECIAL,  EXEMPLARY,  OR CONSEQUENTIAL  DAMAGES  (INCLUDING, BUT  NOT    */
    /*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,    */
    /*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY    */
    /*  THEORY OF  LIABILITY, WHETHER IN CONTRACT, STRICT  LIABILITY, OR TORT    */
    /*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE    */
    /*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.     */
    /*                                                                           */
    /*****************************************************************************/
    
    /*-
     * SPDX-License-Identifier: BSD-2-Clause-NetBSD
     *
     * Copyright (c) 2001, 2002 Mike Barcroft <mike@FreeBSD.org>
     * Copyright (c) 2001 The NetBSD Foundation, Inc.
     * All rights reserved.
     *
     * This code is derived from software contributed to The NetBSD Foundation
     * by Klaus Klein.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     * 1. Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     * 2. Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * THIS SOFTWARE IS PROVIDED BY THE NETBSD FOUNDATION, INC. AND CONTRIBUTORS
     * ``AS IS'' AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED
     * TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED.  IN NO EVENT SHALL THE FOUNDATION OR CONTRIBUTORS
     * BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
     * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
     * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
     * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
     * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
     * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
     * POSSIBILITY OF SUCH DAMAGE.
     *
     * $FreeBSD$
     */
    
    
    #pragma diag_push
    /* 19.4 is issued for macros that are defined in terms of other macros. */
    #pragma CHECK_MISRA("-19.4")
    #pragma CHECK_MISRA("-19.7")
    #pragma CHECK_MISRA("-19.13")
    
    
    
    
    
    
    
    /*
     * ISO/IEC 9899:1999
     * 7.18.2.1 Limits of exact-width integer types
     */
    /* Minimum values of exact-width signed integer types. */
    
    /* Maximum values of exact-width signed integer types. */
    
    /* Maximum values of exact-width unsigned integer types. */
    
    /*
     * ISO/IEC 9899:1999
     * 7.18.2.2  Limits of minimum-width integer types
     */
    /* Minimum values of minimum-width signed integer types. */
    
    /* Maximum values of minimum-width signed integer types. */
    
    /* Maximum values of minimum-width unsigned integer types. */
    
    /*
     * ISO/IEC 9899:1999
     * 7.18.2.3  Limits of fastest minimum-width integer types
     */
    /* Minimum values of fastest minimum-width signed integer types. */
    
    /* Maximum values of fastest minimum-width signed integer types. */
    
    /* Maximum values of fastest minimum-width unsigned integer types. */
    
    /*
     * ISO/IEC 9899:1999
     * 7.18.2.4  Limits of integer types capable of holding object pointers
     */
    
    /*
     * ISO/IEC 9899:1999
     * 7.18.2.5  Limits of greatest-width integer types
     */
    
    /*
     * ISO/IEC 9899:1999
     * 7.18.3  Limits of other integer types
     */
    /* Limits of ptrdiff_t. */
    
    /* Limits of sig_atomic_t. */
    
    /* Limit of size_t. */
    
    /* Limits of wint_t. */
    
    
    #pragma diag_pop
    
    /*-
     * SPDX-License-Identifier: BSD-2-Clause-FreeBSD
     *
     * Copyright (c) 2011 David E. O'Brien <obrien@FreeBSD.org>
     * Copyright (c) 2001 Mike Barcroft <mike@FreeBSD.org>
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     * 1. Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     * 2. Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * THIS SOFTWARE IS PROVIDED BY THE AUTHOR AND CONTRIBUTORS ``AS IS'' AND
     * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
     * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
     * ARE DISCLAIMED.  IN NO EVENT SHALL THE AUTHOR OR CONTRIBUTORS BE LIABLE
     * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
     * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS
     * OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
     * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT
     * LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY
     * OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF
     * SUCH DAMAGE.
     *
     * $FreeBSD$
     */
    
    
    
    typedef	__int16_t		int16_t;
    
    typedef	__int32_t		int32_t;
    
    typedef	__int64_t		int64_t;
    
    
    typedef	__uint16_t		uint16_t;
    
    typedef	__uint32_t		uint32_t;
    
    typedef	__uint64_t		uint64_t;
    
    typedef	__intptr_t		intptr_t;
    typedef	__uintptr_t		uintptr_t;
    typedef	__intmax_t		intmax_t;
    typedef	__uintmax_t		uintmax_t;
    
    
    typedef	__int_least8_t		int_least8_t;
    typedef	__int_least16_t		int_least16_t;
    typedef	__int_least32_t		int_least32_t;
    typedef	__int_least64_t		int_least64_t;
    
    typedef	__uint_least8_t		uint_least8_t;
    typedef	__uint_least16_t	uint_least16_t;
    typedef	__uint_least32_t	uint_least32_t;
    typedef	__uint_least64_t	uint_least64_t;
    
    typedef	__int_fast8_t		int_fast8_t;
    typedef	__int_fast16_t		int_fast16_t;
    typedef	__int_fast32_t		int_fast32_t;
    typedef	__int_fast64_t		int_fast64_t;
    
    typedef	__uint_fast8_t		uint_fast8_t;
    typedef	__uint_fast16_t		uint_fast16_t;
    typedef	__uint_fast32_t		uint_fast32_t;
    typedef	__uint_fast64_t		uint_fast64_t;
    
    _Pragma("diag_push")
    _Pragma("CHECK_MISRA(\"-10.1\")")
    /* GNU and Darwin define this and people seem to think it's portable */
    _Pragma("diag_pop")
    
    _Pragma("diag_push")
    _Pragma("CHECK_MISRA(\"-19.4\")")
    /* Limits of wchar_t. */
    _Pragma("diag_pop")
    
    /* ISO/IEC 9899:2011 K.3.4.4 */
    
    
    _Pragma("diag_pop")
    
    
    
    //
    // Globals
    //
    
    //
    //Task 1 (C) Variables
    
    /*
    #define FILTER_LEN    49
    extern float W[];
    extern long xn;
    extern long yn;
    extern float fDelayLine[];
    */
    
    extern float W1[];
    extern float W2[];
    extern float xn1;
    extern float xn2;
    extern float yn1;
    extern float yn2;
    extern float fDelayLine1[];
    extern float fDelayLine2[];
    
    //
    //Task 2 (C) Variables
    //
    extern long errn;
    //
    //Task 3 (C) Variables
    //
    
    //
    //Task 4 (C) Variables
    //
    
    //
    //Task 5 (C) Variables
    //
    
    //
    //Task 6 (C) Variables
    //
    
    //
    //Task 7 (C) Variables
    //
    
    //
    //Task 8 (C) Variables
    //
    
    //
    //Common (C) Variables
    //
    
    //
    // Function Prototypes
    //
    // The following are symbols defined in the CLA assembly code
    // Including them in the shared header file makes them
    // .global and the main CPU can make use of them.
    //
    __interrupt void Cla1Task1();
    __interrupt void Cla1Task2();
    __interrupt void Cla1Task3();
    __interrupt void Cla1Task4();
    __interrupt void Cla1Task5();
    __interrupt void Cla1Task6();
    __interrupt void Cla1Task7();
    __interrupt void Cla1Task8();
    
    
    
    //
    // End of file
    //
    
    
    
    
    __interrupt void Cla1Task1 ( void )
    {
        __mdebugstop();
      int i;
        float fTemp = 0;
        fTemp = 0;
        #pragma UNROLL(49)
        for(i=49-1;i>0;i--)
        {
        fDelayLine1[i] = fDelayLine1[i-1];
        fTemp += W1[i]*fDelayLine1[i];
        }
        fDelayLine1[0] = (float)xn1; //convert to single precision float
        fTemp += W1[0]*fDelayLine1[0];
        yn1 = (int)fTemp;
        __mdebugstop();
    }
    __interrupt void Cla1Task2 ( void )
    {
        __mdebugstop();
        int i;
        float fTemp = 0;
        fTemp = 0;
        #pragma UNROLL(49)
        for(i=49-1;1>0;i--)
        {
          fDelayLine2[i] = fDelayLine2[i-1];
          fTemp += W2[i]*fDelayLine2[i];
        }
        fDelayLine2[0] = (float)xn2; //convert to single precision float
        fTemp += W2[0]*fDelayLine2[0];
        yn2 = (int)fTemp;
    //    yn2 = xn2; // just to bypass filtering
        __mdebugstop();
    
    }
    
    __interrupt void Cla1Task3 ( void )
    {
    
    }
    
    __interrupt void Cla1Task4 ( void )
    {
    
    }
    
    __interrupt void Cla1Task5 ( void )
    {
    
    }
    
    __interrupt void Cla1Task6 ( void )
    {
    
    }
    
    __interrupt void Cla1Task7 ( void )
    {
    
    }
    
    __interrupt void Cla1Task8 ( void )
    {
    
    }
    //
    // End of file
    //
    

  • Thank you - I've asked the compiler team to take a look.  You should hear back from them soon.

    Regards

    Lori

  • Hi, 

    tasks are not identical. 2nd task for loop has always true condition.

    Edward

  • Edward, 

    I missed the 1>0 condition in your screen shot. Thanks for sending the preprocessed file.

    The warning you are seeing is to be expected for code following an infinite loop. Also, it is not an error.  

    Regards,

    Greg

  • Guys,

    thank you very much for your help! but could you please draw my attention where is the difference? It is definitely some infinite loop because when I run it stuck, but i cannot see it in my code where Cla1Task2 is always true?

    __interrupt void Cla1Task1 ( void )
    {
        __mdebugstop();
      int i;
        float fTemp = 0;
        fTemp = 0;
        #pragma UNROLL(49)
        for(i=FILTER_LEN-1;i>0;i--)
        {
        fDelayLine1[i] = fDelayLine1[i-1];
        fTemp += W1[i]*fDelayLine1[i];
        }
        fDelayLine1[0] = (float)xn1; //convert to single precision float
        fTemp += W1[0]*fDelayLine1[0];
        yn1 = (int)fTemp;
        __mdebugstop();
    }
    __interrupt void Cla1Task2 ( void )
    {
        __mdebugstop();
        int i;
        float fTemp = 0;
        fTemp = 0;
        #pragma UNROLL(49)
        for(i=FILTER_LEN-1;1>0;i--)
        {
          fDelayLine2[i] = fDelayLine2[i-1];
          fTemp += W2[i]*fDelayLine2[i];
        }
        fDelayLine2[0] = (float)xn2; //convert to single precision float
        fTemp += W2[0]*fDelayLine2[0];
        yn2 = (int)fTemp;*/
    //    yn2 = xn2; // just to bypass filtering
        __mdebugstop();
    
    }

    thanks vadim

  • 1st task:

    for(i=FILTER_LEN-1;i>0;i--)

    2nd task:

    for(i=FILTER_LEN-1;1>0;i--)

    i>0 vs 1>0. Hope you see difference now.

    Edward

  • Thank you Edward and Greg.  I swear I looked at that screenshot for a good 10 minutes  LOL.  

    Appreciate the good eyesight :) 

  • Guys, Lori,

    thank you so much! 

    vadim

  • Hi again, I am so sorry, still cannot get them to filter simultaneously even after correction. 
    I call Cla1ForceTask1andWait() from adca_isr and Cla1ForceTask2andWait() from adcb_isr
    But as is, in the attached files adcb_isr does not stop if I put a break point at this interrupt. If I comment out “for” statement in Cla1ForceTask2andWait() than it stops at both adcb_isr and adca_isr.
    Is loop timing can affect interrupt? I checked code with only one task enabled and they both works the same without a problem.

    __interrupt void Cla1Task2 ( void )
    {
        __mdebugstop();
        int i;
        float fTemp = 0;
        fTemp = 0;
    //    #pragma UNROLL(49)
    //    for(i=FILTER_LEN-1;i>0;i--) // only in this case both interrupts work: adca_isr(void), adcb_isr(void);
        {
          fDelayLine2[i] = fDelayLine2[i-1];
          fTemp += W2[i]*fDelayLine2[i];
        }
        fDelayLine2[0] = (float)xn2; //convert to single precision float
        fTemp += W2[0]*fDelayLine2[0];
        yn2 = (int)fTemp;
        __mdebugstop();
    
    }

    thanks vadim

  • That's totally different question!

    You have single CLA, not two. CLA tasks can't run two or more simultaneously, one has to exit to let another one run. 

    Edward

  • vadim said:
    I call Cla1ForceTask1andWait() from adca_isr and Cla1ForceTask2andWait() from adcb_isr
    But as is, in the attached files adcb_isr does not stop if I put a break point at this interrupt.

    Because the c28x is waiting for the task to complete, the C28x will remain in the ISR longer.  If the for() loop in the task is removed, then the C28x stays in the ISR a shorter time.   

    The ADCA ISR has a higher priority than ADCB - so I suspect, with the for(), a new ADCA interrupt is received and then immediately serviced.   Basically the time waiting in ADCA is keeping the CPU from servicing ADCB which is a lower-priority interrupt. 

    Regards

    Lori