Hi Expert,
I will send you a copy with more information through email. Here is general what the question is. Thanks
============================
1) When the input parameter “errorHandle” is set to 0, our program can run normally, and the returned RAM test result is no error, this is ok;
2) When the input parameter “errorHandle” is set to inject an error into RAM, our program cannot run normally. The specific code for injecting error is described as follows;
A. If the settings of “errorHandle” shown in the figure below is correct? If it is not correct, how should we set “errorHandle” to inject an error? Could you help to provide an example?
B. How will the DSP act when a RAM error is detected? Can it continue to operate normally?
modified function STL_March_testRAM