Hello ,
i am using flashapi_ex1_program_autoecc example form c2000 ware and i have made few modification in example code.
/****************************************************************************/
//#############################################################################
//
// FILE: flashapi_ex1_program_autoecc.c
//
// TITLE: Flash programming example for AutoEcc option
//
//! \addtogroup driver_example_list
//! <h1> Flash Programming for AutoECC </h1>
//!
//! This example demonstrates how to program Flash using API's AutoEcc
//! generation option.
//!
//! \b External \b Connections \n
//! - None.
//!
//! \b Watch \b Variables \n
//! - None.
//!
//
//#############################################################################
// $TI Release: F28004x Support Library v1.11.00.00 $
// $Release Date: Sun Oct 4 15:49:15 IST 2020 $
// $Copyright:
// Copyright (C) 2020 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
//
// Include Flash API include file
//
#include "F021_F28004x_C28x.h"
//
// Include Flash API example header file
//
#include "flash_programming_f28004x.h"
//
// Defines
//
// Length (in 16-bit words) of data buffer used for program
#define WORDS_IN_FLASH_BUFFER 0xFF
//
// Globals
//
//Data Buffers used for program operation using the flash API program function
#pragma DATA_SECTION(Buffer,"DataBufferSection");
uint16 Buffer[WORDS_IN_FLASH_BUFFER + 1];
uint32 *Buffer32 = (uint32 *)Buffer;
//
// Prototype of the functions used in this example
//
void Example_Error(Fapi_StatusType status);
void Example_Done(void);
void Example_CallFlashAPI(void);
void FMSTAT_Fail(void);
//
// Main
//
void main(void)
{
//
// Initialize device clock and peripherals
// Copy the Flash initialization code from Flash to RAM
// Copy the Flash API from Flash to RAM
// Configure Flash wait-states, fall back power mode, performance features and ECC
//
Device_init();
//
// Initialize GPIO
//
Device_initGPIO();
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
//
// Notice that Flash API functions are mapped to RAM for execution in this example.
// In F28004x devices that have two banks, Flash API functions may be executed from
// one bank to perform Flash erase and program operations on the other bank.
// Flash API functions should not be executed from the same bank on which erase/
// program operations are in progress.
// Also, note that there should not be any access to the Flash bank on which erase/
// program operations are in progress. Hence below function is mapped to RAM for
// execution.
//
Example_CallFlashAPI();
}
//*****************************************************************************
// Example_CallFlashAPI
//
// This function will interface to the flash API.
// Flash API functions used in this function are executed from RAM in this
// example.
//*****************************************************************************
#ifdef __cplusplus
#pragma CODE_SECTION(".TI.ramfunc");
#else
#pragma CODE_SECTION(Example_CallFlashAPI, ".TI.ramfunc");
#endif
void Example_CallFlashAPI(void)
{
uint32 u32Index = 0;
uint16 i = 0;
Fapi_StatusType oReturnCheck;
Fapi_FlashStatusType oFlashStatus;
Fapi_FlashStatusWordType oFlashStatusWord;
//
// Note that wait-states are already configured in the Device_init().
// However, if INTOSC is used as the clock source and
// if the CPUCLK falls in the range (97,100] (check other ranges given in DS),
// then an extra wait state is needed for FSM operations (erase/program).
// Hence, below function call should be uncommented in case INTOSC is used.
// At 100MHz, execution wait-states for external oscillator is 4 and hence
// in this example, a wait-state of 5 is used below.
// This example is using external oscillator as the clock source and hence
// below is commented.
//
// This wait-state setting impacts both Flash banks. Applications which
// perform simultaneous READ/FETCH of one bank and PROGRAM or ERASE of the other
// bank must use the higher RWAIT setting during the PROGRAM or ERASE operation. OR
// use a clock source or frequency with a common wait state setting
// Example: Use 97MHz instead of 100MHz if it is acceptable for the application.
//
// In case, if user application increments wait-state before using API,
// then remember to revert back to the original wait-state after the API usage
// to avoid extra wait-state during application execution from Flash.
//
//
// Flash_setWaitstates(FLASH0CTRL_BASE, 5);
// Initialize the Flash API by providing the Flash register base address
// and operating frequency.
// This function is required to initialize the Flash API based on System frequency
// before any other Flash API operation can be performed.
// This function must also be called whenever System frequency or RWAIT is changed.
oReturnCheck = Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS, 100);
if(oReturnCheck != Fapi_Status_Success)
{
// Check Flash API documentation for possible errors
Example_Error(oReturnCheck);
}
// Initialize the Flash banks and FMC for erase and program operations.
// Fapi_setActiveFlashBank() function sets the Flash banks and FMC for further
// Flash operations to be performed on the banks.
// Note: It does not matter which bank is passed as the parameter to initialize.
// Both Banks and FMC get initialized with one function call unlike F2837xS.
// Hence there is no need to execute Fapi_setActiveFlashBank() for each bank.
// Executing for one bank is enough.
oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);
if(oReturnCheck != Fapi_Status_Success)
{
// Check Flash API documentation for possible errors
Example_Error(oReturnCheck);
}
// Erase Flash Bank0 sector6
oReturnCheck = Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector,
(uint32 *)Bzero_Sector6_start);
// Wait until FSM is done with erase sector operation
while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){}
if(oReturnCheck != Fapi_Status_Success)
{
// Check Flash API documentation for possible errors
Example_Error(oReturnCheck);
}
// Read FMSTAT register contents to know the status of FSM after
// erase command to see if there are any erase operation related errors
oFlashStatus = Fapi_getFsmStatus();
if(oFlashStatus != 0)
{
// Check Flash API documentation for FMSTAT and debug accordingly
// Fapi_getFsmStatus() function gives the FMSTAT register contents.
// Check to see if any of the EV bit, ESUSP bit, CSTAT bit or
// VOLTSTAT bit is set (Refer to API documentation for more details).
FMSTAT_Fail();
}
// Do blank check
// Verify that Bank0 sector6 is erased. The Erase command itself does a verify as
// it goes. Hence erase verify by CPU reads (Fapi_doBlankCheck()) is optional.
oReturnCheck = Fapi_doBlankCheck((uint32 *)Bzero_Sector6_start,
Sector8KB_u32length,
&oFlashStatusWord);
if(oReturnCheck != Fapi_Status_Success)
{
// Check Flash API documentation for error info
Example_Error(oReturnCheck);
}
// A data buffer of max 8 16-bit words can be supplied to the program function.
// Each word is programmed until the whole buffer is programmed or a
// problem is found. However to program a buffer that has more than 8
// words, program function can be called in a loop to program 8 words for
// each loop iteration until the whole buffer is programmed.
//
// Remember that the main array flash programming must be aligned to
// 64-bit address boundaries and each 64 bit word may only be programmed
// once per write/erase cycle. Meaning the length of the data buffer
// (3rd parameter for Fapi_issueProgrammingCommand() function) passed
// to the program function can only be either 4 or 8.
//
// Program data in Flash using "AutoEccGeneration" option.
// When AutoEccGeneration opton is used, Flash API calculates ECC for the given
// 64-bit data and programs it along with the 64-bit main array data.
// Note that any unprovided data with in a 64-bit data slice
// will be assumed as 1s for calculating ECC and will be programmed.
//
// Note that data buffer (Buffer) is aligned on 64-bit boundary for verify reasons.
//
// Monitor ECC address for Bank0 Sector6 while programming with AutoEcc mode.
//
// In this example, 0xFF+1 bytes are programmed in Flash Bank0 Sector6
// along with auto-generated ECC.
//
// Fill a buffer with data to program into the flash.
//
for(i=0; i <= WORDS_IN_FLASH_BUFFER; i++)
{
Buffer[i] = i;
}
for(i=0, u32Index = Bzero_Sector6_start;
(u32Index < (Bzero_Sector6_start + WORDS_IN_FLASH_BUFFER)) &&
(oReturnCheck == Fapi_Status_Success); i+= 8, u32Index+= 8)
{
oReturnCheck = Fapi_issueProgrammingCommand((uint32 *)u32Index, Buffer+i, 8,
0, 0, Fapi_AutoEccGeneration);
// Wait until the Flash program operation is over
while(Fapi_checkFsmForReady() == Fapi_Status_FsmBusy);
if(oReturnCheck != Fapi_Status_Success)
{
// Check Flash API documentation for possible errors
Example_Error(oReturnCheck);
}
// Read FMSTAT register contents to know the status of FSM after
// program command to see if there are any program operation related errors
oFlashStatus = Fapi_getFsmStatus();
if(oFlashStatus != 0)
{
//Check FMSTAT and debug accordingly
FMSTAT_Fail();
}
}
// Example is done here
Example_Done();
}
//******************************************************************************
// For this example, just stop here if an API error is found
//******************************************************************************
void Example_Error(Fapi_StatusType status)
{
// Error code will be in the status parameter
__asm(" ESTOP0");
}
//******************************************************************************
// For this example, once we are done just stop here
//******************************************************************************
void Example_Done(void)
{
__asm(" ESTOP0");
}
//******************************************************************************
// For this example, just stop here if FMSTAT fail occurs
//******************************************************************************
void FMSTAT_Fail(void)
{
// Error code will be in the status parameter
__asm(" ESTOP0");
}
//
// End of File
//
in above code just i am writing 255 bytes of data from 0x86000 location,it is writing perfectly
But after Power on Reset (turn off and on the target board) data is not available (Why?).
and How should I differentiate that i am doing program flash (which is not retain after POR),and Data flash (which should retain after POR) By using memory locations.
Please suggest me regarding this query
regards
chandan