Part Number: TMS320F28027F
Hi everyone!
Good Day!
in some cases like fan or pumps application I saw 2 or 3 motors or more connected to one drive ,
in V/F system is possible because Angle of the rotor are not put in to account .
question1: is that would it be possible to do this kind of connection in FOC mode?
question 2: Assuming we have two motor with FOC control method, if we load one what is going to happed for the next one?
Question 3: as far as I know in FOC ,the control would be torque dynamic so if we load one motor the next one would spin more is that right?
thanks for attention
Dave.