Part Number: TMS320F28388D
Hello,
We are using F28388D, the ePWM clock is 200MHz(5ns step).
Our Purpose is to ensure the accuracy of 1ns step resolution for Dead band high-resolution.
According to TRM manual, there are two ways to calculate in HR mode.
1. HR register is manually scaled by calculations in application software
2. HR register is automatically scaled by the MEP scale factor in the HRMSTEP register (SFO)
If using SFO in our system, we have concern that the MEP step size changing may cost unexpected behavior.
To avoid this, we may consider to calculate manually by software.
Here are my questions.
- In TRM manual, I see the typical MEP step size is on the order of 150 ps, is it possible to set the MEP step size to 250ps?
- If possible, is it guaranteed always calculating with this step size?
- If there is a shift from original step size 250ps, how to confirm?
- It is said using SFO can vary MEP step size based on worst-case process parameters, operating temperature, and voltage,
If scaling manually with fixed step size, what could happen in the worst-case process parameters, operating temperature, and voltage?
Thank you.
Best Regards,
Wenjing