its a printer cable through which i m
connecting my F2812 kit to the computer. i made a model in simulink
which contains 28xx ADC block , a scope , target preferecnce. i m
trying to to trace a signal given at ADC channel A pin 0,.i build the
model using grt.tlc and also ccslink_ide.tlc both works fine build is
completed with 0 error in normal mode. then i changed mode to external
and build it again. i do have a doubt in TCP/ip mex file argument as i
m using only one system not two. i search a lot but i can't get how
to pass mexfile argument which may be the reason why i m facing
problem to 'connect to target,
i need a help my work is being stopped due to this problem