Part Number: TMS320F28035
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
I noticed that in C2000Ware there are two sets of "drivers" available: device_support and driverlib.
The "device_support" is based on bit-level access to configuration registers and have defines for all peripheral (module) registers.
The "driverlib" does not have configuration register definitions, but has more configuration functions with a lot of macro constants and enums.
Which one is recommended to be used in new projects? In other words, which of the two will receive support in the future?
Moreover, it seems that "driverlib" is not available for F2803x in the latest C2000Ware release. Is there a plan to provide "driverlib" for F2803x in the future, or we have no other option but to use "device_support" in that case?