Part Number: TMS320F28379D
Hi experts,
I'd like to generate ECC during the link step.
I created the linker command file by the method described in No.39 of the link below.
However, I get the following error:
"../2837x_FLASH_lnk_cpu1.cmd", line 150: error #10395: not a valid ECC algorithm parameter name
What's wrong?
I have attached the linker command file I created. Could you give me some advice on this.
MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASHA : origin = 0x080000, length = 0x002000, vfill = 0xFFFF /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000, vfill = 0xFFFF /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000, vfill = 0xFFFF /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000, vfill = 0xFFFF /* on-chip Flash */
FLASH_A_ECC : origin=0x1080000, length=0x400, ECC = { /* ECC Specifier */
input_range = FLASHA,
input_page = 0,
algorithm = C2000_Algo,
fill = true
} /* End of ECC Specifier */
FLASH_B_ECC : origin=0x1080400, length=0x400, ECC = {
input_range = FLASHB,
input_page = 0,
algorithm = C2000_Algo,
fill = true
}
FLASH_C_ECC : origin=0x1080800, length=0x400, ECC = {
input_range = FLASHC,
input_page = 0,
algorithm = C2000_Algo,
fill = true
}
FLASH_D_ECC : origin=0x1080C00, length=0x400, ECC = {
input_range = FLASHD,
input_page = 0,
algorithm = C2000_Algo,
fill = true
}
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.text : >> FLASHB | FLASHC | FLASHD PAGE = 0, ALIGN(4)
my_param : > FLASHG PAGE = 1, ALIGN(4)
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
#endif
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : >> RAMLS5 | RAMGS0 | RAMGS1 PAGE = 1
.esysmem : > RAMLS5 PAGE = 1
/* Initalized sections go in Flash */
.econst : >> FLASHD PAGE = 0, ALIGN(4)
.switch : > FLASHB PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
Filter_RegsFile : > RAMGS0, PAGE = 1
SHARERAMGS0 : > RAMGS0, PAGE = 1
SHARERAMGS1 : > RAMGS1, PAGE = 1
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
}
ECC
{
C2000_Algo: parity_mask = 0xFC Mirroring = F021
} /* End of ECC Directive */
/*
//===========================================================================
// End of file.
//===========================================================================
*/
Best regards,
Sasaki