Part Number: TMS320F2806
Other Parts Discussed in Thread: UNIFLASH
Hi there,
I'm trying to program a TMS320F2806 with a XDS200 JTAG Emulator but I constantly get the following error:
[ERROR] C28xx: Trouble Reading Register PC: (Error -1156 @ 0xA) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 9.3.0.00032)
I tried this using UniFlash 6.2.0.3059 as well as Code Composer 10.2.0.00009.
When using Code Composer I can run a test when configuring the setup which passes successfully.
In UniFlash I'm also able to read the memory. However, when I try to program the above error occurs. Any suggestion on what I could be doing wrong?
I also tried resetting the device from uniflash by opening the resetting options. Again I get the Error 1156 (as above) but additionally the error "Could not read register ST1: target is not connected (ST1|0x0200)"
I have to say though that the whole change is insanely unstable. Pretty much after every attempt I have to restart the program, reconnect the XDS200 and power cycle the device. Otherwise UniFlash just seams to crash.
Any help would be highly appreciated.
Thanks!