Other Parts Discussed in Thread: TMS320F28335
Hey Ti Guys,
I'm using the PWM Module of the tms320f28335 - the Manual discribe that a PWM synchronization of the Phase and Timebase is possible, but I do not know if it is possible to syncronize a compleat PWM Sectoion with the TMS like an Atmel ?
Example:
I got two PWMs: PWMX1 and PWMX2. The first PWM works with 75 Duty, the Second with 25% from one to the other there is a phase of 180° - so can I switch in a State the output of PWM 1 to PWMX1 and PWM2 to PWMX2, and in the next state PWM3 to PWMx1 and PWM2 to PWMX1 ?
like the pdf (Blue PWMX1, Red PWMX2)
Thanks,
Heiko