This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: PLL VCO max frequency

Part Number: TMS320F28377D


Hello everyone

In the F2837xD TRM (SPRUHM8) part 2.7.6.1 "Choosing PLL Settings it's said":

Many combinations of multiplier and divider can produce the same output frequency. However, the
product of the reference clock frequency and the multiplier (known as the VCO frequency) must be in the
range specified in the data manual.

However in Datasheet (SPRS880) there is no mention of VCO frequency. There is a table 8.9.3.2.2.1 "Internal Clock Frequencies". There is a PLLRAWCLK frequency in the table - is it the VCO frequency?
Does it mean that maximum VCO frequency is 400 MHz?

Thanks