Part Number: TMS320F28388D
Hello All
So I am going to create I-RTOS(DSP/BIOS) project for TMS320F28388x
I Have installed
1) CCS 10.0.0.00010
2) xdceools_3_61_01_25_core
3) BIOS_6_76_01_12
Everything is installed in C:/ti directory
and I have leant documents
1) TI-RTOS 2.16 for C2000 (SPRUHU3D)
2) Huw to Develop a Project With TI SYS/BIOS (SPRABW1 – April 2014)
Nothing helpful .
The Project Window of CCS does not contain Project templates SYS/BIOS , described in second document.
The my Resource Explorer has other appearance (See the attachment) and does not contain examples RTOS (SYS/BIOS) for F28M35x Concerto as it described in first document nor for F2838x as I could suppose.
The question - Which document I have to use to create project of TI RTOS (SYS/DSP)specially for TMS320F28388D for ARM core ? , where I can load examples of project creation and for driver creation for ARM core from?
I have one example which called tcpEchoF2838X but it has some bugs (or features ) but it does not show me how to create project.
Best regards
Andrii